2404635_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2404635_en-US

2404635_en-US

Inquiry: NXP EasyEVSE for ISO 15118-20 EVCC Simulation and SECC Testing

Hi 

We are developing a custom charger-side ISO 15118-20 SECC.

We are considering the NXP EasyEVSE platform as an EV-side simulator to test our charger without requiring a real vehicle. We understand that the MIMXRT1064-EVK would run the EVCC software, while the EVSE-SIG-BRD2X and Green PHY hardware would provide the CP/PE and PLC connection to our charger.

Could you please confirm:

  1. Whether this platform/hardware can operate in EV/EVCC mode and test a custom SECC.
  2. Whether it supports ISO 15118-20 AC and AC-BPT.
  3. Whether it can test CP states and 5% PWM, SLAC, SDP, TCP/TLS, authorization, service discovery, schedule exchange, charging loop and session stop.
  4. Whether simulated EV values such as Present SoC, Target SoC and charging/discharging power limits can be configured.
  5. The exact EV-side hardware BOM, including the correct signal board, Green PHY board, cables and part numbers.
  6. Whether the required SEVENSTAX software is included or requires a separate evaluation licence.
  7. Whether QA/test TLS certificates and a secure element are required for evaluation.
  8. Which EV parameters and message fields can be modified;
  9. Whether charge and discharge power can be changed dynamically during a session;

This setup is intended only for laboratory development and interoperability testing.


Best regards,

Tags (1)
No ratings
Version history
Last update:
Friday
Updated by: