2404460_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2404460_en-US

2404460_en-US

NXP S32K312 CAN0 – FIRC vs. FXOSC Clock Source Causing CAN Errors

Hi everyone,

I am using CAN0 on the S32K312 at 500 kbps with an 87.5% sampling point.

Initially, I set up CAN0 to use the internal FIRC_CLK as the clock source. When I connected the S32K312 to a network with multiple CAN nodes, I noticed a lot of CAN error frames.

I then switched the CAN clock source from FIRC_CLK to the external FXOSC_CLK while keeping the CAN bitrate and sampling point the same. After this change, the communication became stable, and I stopped seeing the error frames.

Could anyone help me understand why switching the clock source from FIRC_CLK to FXOSC_CLK would fix the CAN errors?

Re: NXP S32K312 CAN0 – FIRC vs. FXOSC Clock Source Causing CAN Errors

Hello @Karthik_R,

Usually, FIRC clock is not recommended for FlexCAN communication, as accuracy is over the ~1% requirement according to CAN protocol (ISO 11898-1). You can see from S32K3's Data Sheet that FIRC's deviation is +- 5%.

Recommendation is to use either FXOSC or PLL running from XOSC. You can refer to FlexCAN Bit Timing Calculation document, and MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD bit timing calculation tool for clock and timing calculations.

Hope this is clear.

Best regards,
Julián


タグ(1)
評価なし
バージョン履歴
最終更新日:
金曜日
更新者: