2403977_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2403977_en-US

2403977_en-US

The S32 IDE development environment RTD plugin cannot be installed.

To develop software for the S32Z280 processor, you need to install the S32ZE RTD plugin in the S32 IDE development environment. However, installation fails in the environment, as shown in Figure 1. It cannot be downloaded from the NXP website, which requires a license. Please provide information on how to obtain the license. Thank you.

Re: S32 IDE开发环境RTD插件无法安装

You're welcome. Feel free to contact me anytime if you have any questions!

Re: S32 IDE开发环境RTD插件无法安装The first link required account login, and the download path for the installation package was not displayed after logging in. The second link allowed me to successfully download the installation package after accessing the "Car Package Manager," thank you.Re: S32 IDE开发环境RTD插件无法安装

Hi, Flynn_T

1. Can you download it from this link? The latest RTD version should be 2.0.1 QLP01; version 1.1.45, which you mentioned, is not listed. Also note that the 2.0.1 QLP01 RTD requires S32DS IDE version 3.6.1.

Design: Product Information: Automotive SW - S32Z/E - Real Time Drivers (RTD)

Joey_z_0-1786528248987.png

2. You can also check this link to see if you can download it.

Automotive Package Manager | NXP Semiconductors

BR

Joey

Re: S32 IDE开发环境RTD插件无法安装

Hi, BR Joey
I'm using S32 IDE version 3.6.10. The required RTD version is 1.1.45. I couldn't find a download link for the S32Z/E RTD plugin on the NXP official website. Please provide a download link.


Best Regard

Flynn_T

Re: S32 IDE开发环境RTD插件无法安装

Hi, Flynn_T

What version of S32 IDE are you using? What version of RTD are you using?

Loading the S32Z/E RTD plugin in the IDE generally does not require a license.

BR

Joey

Tags (1)
No ratings
Version history
Last update:
Thursday
Updated by: