I'm currently debugging an .imx95 15x15 packaged DDR5 and have encountered a problem. DDR5: RS2G32LO5D4FB-31BT1. I used ConfigTools for i.MX 26.06, verification, using the .bin file compiled with lpddr5_timing.c, during flashing, the M33 core showed DDR...OEI: done, err = -12. I reduced the DDR speed to 1866 MT/s, but I still got a -1 error.3. I noticed that the SDK does not include an official version of the IMX9596 15x15 DDR5.yrj_0-1786433338089.png
yrj_1-1786433341485.png
Hi @yrj
The IMX95 does not support DDR5.
B.R
Is it LPDDR5? Does it support it?
HI @yrj
Yes, it supports LPDDR5 and LPDDR4X.
B.R
The part is LPDDR5 and you may need to review the schematics