2403508_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2403508_en-US

2403508_en-US

Scrubbing ECC RAM

MCU: S32K148

Driver: RTD 3.0.0

OS: Bare metal


With the above MCU, is there a way of 'scrubbing' the ECC SRAM? 'Scrubbing' means that if a correctable error is detected, the SRAM cell is updated with the correct value if the user configures some appropriate registers. Some competing products such as TI Hercules have this feature.

Re: Scrubbing ECC RAMThank you very much for the feedback.Re: Scrubbing ECC RAM

S32K1 devices do not support a hardware SRAM scrubbing mechanism that would automatically write corrected data back to memory after a correctable ECC event. A software-based implementation is also not feasible, as single-bit SRAM ECC correction events are not reported by the ERM, so the application cannot identify the affected memory location.

While the S32K3 family also does not provide automatic SRAM scrubbing, it does report single-bit ECC events, which gives the application visibility into these errors and enables implementation of more advanced fault-handling strategies.

タグ(1)
評価なし
バージョン履歴
最終更新日:
水曜日
更新者: