2403486_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2403486_en-US

2403486_en-US

mc9s08qg8 drivers

device manager:

Jungo connectivity

WinDriver:      Windows cannot verify the digital signature for the drivers required for this device. A recent hardware or software change might have installed a file that is signed incorrectly or damaged, or that might be malicious software from an unknown source. (Code 52)

 
pemicrowindvr:    This device is working properly.
 
These r the drivers i have in jungo!!!
 
ur input:
 
In USB Multilink Universal and USB Multilink Universal FX Technical Summary [USBMLUNIVERSALFX] documentation Chapter 6 Driver Installation mention that a copy of the driver installation program may be downloaded from P&E page "Support Center">Downloads. if you need an updated driver.   Best Regards,
 
What do u mean by this. Is this where i can get my BDM driver for my Wiztronics.com P&E interface board?
Re: mc9s08qg8 drivers

Hello,

From the other post, I was referring that, as you are using P&E USB multilink Universal, the support page could redirect you to download a patch or an upgrade to your driver, I found these resources that could maybe help you if you have an incorrectly driver.

In these page, its mentioned some patches for CodeWarrior v10.2 or higher and v6.3, to add support for PE hardware if is not detected by the operating system. PEmicro FAQ ID 211

Another option USB Multilink Resources Install Is a resource package for USB Multilink Universal, for when running older software.

Also could you help us share which exact version of USB multilink Universal are you using?

I could not guarantee this will work, since it’s a partner page, but it could redirect you in how to look for a driver correction for your issue, hope this information was helpful and let me know if that work for you

Best Regards.

タグ(1)
評価なし
バージョン履歴
最終更新日:
水曜日
更新者: