2403280_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2403280_en-US

2403280_en-US

S32K358 chip temperature

When the S32K358 is operating at 240MHz and the ambient temperature is 24℃, the internal temperature of the MCU is read as 60℃. This IC temperature was measured with copper plating for heat dissipation on the PCB. Is this temperature normal?

Re: S32K358的芯片温度Yes, it's the measurement result from the internal temperature sensor of the IC. The application scenario is BMS (Battery Management System).Re: S32K358的芯片温度

Hi @liyongfeng 

Could you please use the internal Temperature Sensor (TempSense) to measure the MCU junction temperature (Tj)?

Tj represents the temperature of the silicon die and is the most critical thermal parameter for device operation. This value must always remain below the limits specified in the Thermal Operating Characteristics section of the S32K3xx Data Sheet, Rev. 14.


BR, VaneB

Re: S32K358的芯片温度

Within the chip's normal operating temperature range, what specific functions do you use this chip for?

タグ(1)
評価なし
バージョン履歴
最終更新日:
木曜日
更新者: