Hi @rejust ,
Thank you so much for your interest in our products and for using our community.
Yes, from the default FRDM-IMXRT1186 schematic, the design is intended to meet this sequencing requirement.
R337 is DNP by default, so VDDA_ADC_3P3 is not directly tied to VDD_3V3 through the 0 Ω bypass path. Instead, VDDA_ADC_3P3 is supplied through the U17 MOSFET sequencing circuit. This circuit is controlled by the VDDA_ADC_1P8 / ADC_1V8_IN rail, so VDDA_ADC_3P3 is enabled only after VDDA_ADC_1P8 is established.
For production design, a PMIC is not mandatory. Any reliable sequencing method is acceptable, such as a PMIC, LDO/load switch with EN control, or a MOSFET sequencing circuit, as long as the timing at the SoC pins meets the datasheet requirement.
Wish it helps you
Best Regards
May