my P&E USB multilink Universal Interface MC908JB8 chip needs a BDM driver to download my code to my MCS08QG8 chip.Otherwise I need a P&E USB multilink Universal board to load my MC9S08QG8 chip.And the board runs about $200.I would prefer to get a BDM driver for my Lenovo USB port.U say the BDM driver is in the CW v6.3 development software code!I loaded the CW v6.3 code but it will not install, because the "OS is wrong".the orginal OS was for my xp computer, but i am running windows 11 now and the cw v6.3 will not install on that OS.HELPPPPPPPPP!!!!!!!!!
well, i need the BDM interface for my MC9s08qg8 chip. i am trying to use Windows 11 with a BDM USB driver. Can i create a VM and accomplish this task, or is that path a dead end, too.