If you're shopping for an electric bike, one of the biggest decisions is choosing between a mid-drive motor and a hub motor.
Neither design is automatically better. Mid-drive motors are especially good at using the bike's gears to handle steep hills and technical terrain, while hub motors are simpler, usually more affordable, and require less drivetrain maintenance.
For many everyday riders, a good hub motor provides more than enough performance. Riders dealing with serious hills, mountain trails, or demanding cargo use may benefit more from a mid-drive system.
Here's a practical comparison.
Mid-Drive vs Hub Motor at a Glance
Feature Mid-Drive Motor Hub Motor
Motor Location Around the crank/pedals Front or rear wheel hub
Best For Hills, trails, technical riding Commuting, leisure, mixed everyday riding
Hill Performance Excellent Good to excellent depending on torque
Weight Distribution Very balanced More weight at one wheel
Drivetrain Wear Higher Lower
Maintenance More involved Generally simpler
Flat Tire Repair Usually easier Motor-wheel removal can be harder
Pedaling Feel Often very natural Depends heavily on sensor tuning
Price Usually higher Usually more affordable
What Is a Mid-Drive Motor?
A mid-drive motor is positioned near the bottom bracket, where the pedals and crankset meet the frame.
Instead of directly turning a wheel, the motor sends power through the bicycle's drivetrain. That means the motor can take advantage of the bike's gears in much the same way the rider does.
Shift into a lower gear for a steep climb, for example, and the motor can operate at a more favorable speed while producing strong climbing assistance.
This is the biggest reason mid-drive systems are popular on performance-oriented electric mountain bikes and other bikes designed for demanding terrain.
Pros of Mid-Drive Motors
1. Excellent Hill-Climbing Performance
This is probably the strongest argument for a mid-drive.
Because motor power passes through the bicycle's gears, you can select a lower gear when climbing. This helps the motor operate efficiently instead of forcing it to pull the bike uphill at very low motor RPM.
For riders living in extremely hilly areas, this can make a noticeable difference.
However, don't assume that every mid-drive automatically climbs better than every hub motor. Motor torque, controller tuning, rider weight, gearing, tire size, and total bike weight all matter.
A strong 750W geared hub motor with high torque can still be an excellent hill climber for normal roads and moderate trails.
2. Better Weight Distribution
A mid-drive motor places its weight low and near the center of the bicycle.
That generally gives the bike more neutral handling because there isn't a large motor concentrated inside the front or rear wheel.
The advantage becomes especially noticeable during technical mountain biking, quick direction changes, and riding over uneven terrain.
3. Efficient Use of Motor Power
Because the motor can use the bicycle's gears, a mid-drive system can keep the motor operating in a more efficient RPM range.
This can improve efficiency on routes involving frequent elevation changes.
It doesn't necessarily mean a mid-drive will always have longer range, though. Battery capacity, speed, tire pressure, rider weight, temperature, elevation, wind, and assist level can easily have a larger effect on real-world range.
4. Natural Pedaling Experience
Many higher-end mid-drive systems are paired with torque sensors.
A torque sensor measures how hard you're pushing on the pedals and adjusts motor assistance accordingly.
Push harder and you receive more assistance. Pedal gently and the motor responds more gently.
The result can feel surprisingly similar to riding a normal bicycle—except that you suddenly have much stronger legs.
Cons of Mid-Drive Motors
1. More Drivetrain Wear
The same feature that gives a mid-drive its climbing advantage also creates one of its biggest disadvantages.
Both the rider and motor are sending power through components such as the:
Chain
Chainring
Cassette
Derailleur system
High motor torque combined with poor shifting habits can accelerate drivetrain wear.
If you regularly shift gears while the motor is delivering maximum power, chains and cassette teeth may wear substantially faster.
2. More Expensive
Mid-drive systems generally cost more.
The motor must be integrated around the crank area, and the frame often needs to be designed specifically around that drive unit.
For riders who mainly travel on pavement or relatively gentle terrain, paying the premium may not provide enough practical benefit.
3. Shifting Technique Matters
Mid-drive riders need to think more carefully about gears.
Starting a steep hill in a very high gear and then shifting under heavy motor load isn't ideal. Good riding technique involves selecting an appropriate gear before the drivetrain becomes heavily loaded.
For experienced cyclists, this quickly becomes natural. For beginners, there can be a learning curve.
4. A Broken Chain Can Become a Bigger Problem
Because a mid-drive transfers motor power through the chain, drivetrain failure can potentially leave you unable to use the motor to drive the rear wheel.
A throttle-equipped hub-drive bike can have an advantage here because its motor operates independently from the bicycle chain.
What Is a Hub Motor?
A hub motor is built directly into the center of the front or rear wheel.
Rear hub motors are particularly common on modern electric bikes.
Instead of sending power through the chain and cassette, the motor directly rotates the wheel. This makes the system mechanically straightforward and separates motor power from the traditional bicycle drivetrain.
Several Himiway models use powerful hub-drive configurations. Bikes such as the Himiway D5 2.0 Series demonstrate why hub motors remain popular on practical fat-tire e-bikes: they can combine substantial torque with relatively straightforward operation.
Pros of Hub Motors
1. Simple and Low-Maintenance Design
One of the biggest advantages is simplicity.
The motor doesn't normally send its power through the bicycle chain or cassette. Your drivetrain therefore only has to handle your pedaling force rather than your pedaling force plus motor output.
For riders who want an e-bike for commuting, weekend rides, errands, or recreation, this simplicity is valuable.
2. Strong Everyday Performance
It's outdated to think that hub motors are only suitable for flat roads.
Modern geared hub motors can produce substantial torque.
For example, the Himiway D5 2.0 uses a 750W geared hub motor rated at 90 Nm of torque. That's the kind of specification designed to provide strong acceleration and useful climbing assistance rather than simply cruising along perfectly flat bike paths.
The D5 2.0 20" combines the same general idea with 20-inch fat tires and full suspension, giving riders a compact platform designed around comfort and maneuverability.
For normal hills, neighborhood streets, gravel roads, and recreational trails, a well-designed hub motor can be more than capable.
3. Lower Purchase Cost
Hub motors are generally less complicated and less expensive for manufacturers to integrate into an e-bike.
That can allow more of the bike's budget to go toward other features such as:
Larger batteries
Hydraulic brakes
Better suspension
Integrated lighting
Fat tires
Higher payload capacity
This is one reason hub-drive bikes can offer very attractive specifications for the money.
4. Less Stress on the Chain and Cassette
Since motor power goes directly to the wheel, the chain doesn't have to transmit the motor's full torque.
That can mean longer drivetrain component life compared with a powerful mid-drive bike, assuming both bikes are maintained properly.
5. Throttle Operation Can Be Useful
On compatible hub-drive e-bikes equipped with a throttle, motor operation doesn't necessarily depend on the bicycle drivetrain.
This can be convenient when starting from a stop, briefly moving through an intersection, or getting the bike moving when carrying a load.
It also provides an important mechanical advantage: a broken chain doesn't necessarily prevent the motor from moving the bicycle.
Cons of Hub Motors
1. Less Efficient on Extreme Climbs
A conventional hub motor can't take advantage of the bicycle's cassette in the same way a mid-drive can.
On a long and very steep climb, the motor may be forced to operate at low speed under heavy load.
That can increase heat generation and energy consumption.
For occasional hills this might not matter much. For riders climbing steep mountain roads every day, it becomes much more important.
2. Heavier Rear or Front Wheel
The motor adds substantial mass to whichever wheel contains it.
Most powerful e-bikes use rear hub motors, so the rear of the bicycle can feel heavier when lifting or servicing it.
You may notice this more when carrying the bike upstairs than when actually riding it.
3. Flat Tire Repairs Can Be More Complicated
A hub-motor wheel isn't quite as easy to remove as an ordinary bicycle wheel.
You may need to disconnect the motor cable and deal with a significantly heavier wheel.
For that reason, maintaining correct tire pressure and using puncture-resistant tires can be particularly worthwhile on hub-drive e-bikes.
What About Himiway eBikes?
Himiway ebikes is a useful example because many of its bikes emphasize powerful hub-drive systems rather than automatically using a mid-drive simply because it sounds more premium.
Models such as the Himiway D5, D5 Pro, D5 2.0, D5 2.0 ST, D5 2.0 Camo, D5 2.0 20", C3, A7, A7 Pro, D7, and D7 Pro target different types of riding, so the important point is to look at the complete bike rather than judging it solely by motor location.
For example, a rider considering a D5 2.0 may care about strong torque, fat-tire traction, suspension comfort, range, and everyday reliability more than achieving the lightest possible drivetrain.
The D5 2.0 20" is particularly interesting for riders who value easier maneuverability and comfort. Its smaller 20-inch wheels, 4-inch tires, full suspension, and low center of gravity create a very different riding experience from a traditional large-wheel mountain e-bike.
The A7 and A7 Pro, meanwhile, are more relevant to riders prioritizing urban transportation and everyday usability.
And the C1 Kids belongs in a completely different category. For younger riders, controllability, appropriate sizing, speed management, braking, and adult supervision are far more important than chasing maximum motor torque.
This highlights an important lesson:
Don't choose an e-bike based on the motor alone.
What Riders Actually Notice
Specifications are useful, but everyday riding tends to make the differences much simpler.
A well-tuned hub-drive bike often feels effortless during normal commuting. You pedal, assistance arrives, and you keep moving without constantly thinking about gears.
A good mid-drive tends to reward riders who actively use their gears. When approaching a hill, shifting down allows the motor and rider to work together efficiently. On technical terrain, the centered weight can also make the bicycle feel more balanced.
The difference becomes much less dramatic when you're cruising at moderate speeds on a flat bike path.
That's why paying substantially more for a mid-drive isn't automatically worthwhile for every rider.
Which Motor Is Better for Hills?
Mid-drive wins for serious climbing.
If your normal rides include long, steep mountain climbs, a mid-drive's ability to use the bike's gearing is a major advantage.
But there's an important distinction between "hills" and "extreme hills."
Most people aren't climbing mountain passes every morning.
A high-torque geared hub motor can handle typical neighborhood hills, rolling countryside, gravel roads, and moderate trail climbs very well. That's why bikes such as the Himiway D5 2.0 can make sense for riders who want climbing ability without moving to a more expensive mid-drive platform.
Which Is Better for Commuting?
For typical commuting, I'd give the advantage to the hub motor.
It's simple, relatively inexpensive, puts less motor-related stress on the bicycle drivetrain, and provides plenty of assistance for normal urban riding.
If your commute involves extremely steep terrain, however, a mid-drive becomes more attractive.
Which Is Better for Mountain Biking?
For serious technical mountain biking, I'd choose a mid-drive.
The centered motor position improves weight distribution, while access to the bike's gearing helps during steep and technical climbs.
For gravel roads, forest paths, dirt roads, camping trips, and relatively moderate recreational trails, a powerful fat-tire hub-drive bike can still be an excellent choice.
Which Is Better for Beginners?
For many beginners, a hub-drive e-bike makes more sense.
There's less need to think about keeping the motor in the correct gear, drivetrain maintenance is straightforward, and prices are often more approachable.
However, motor type isn't the only factor affecting ease of use.
Frame geometry, wheel size, bike weight, standover height, throttle behavior, torque or cadence sensing, brakes, and suspension can make an even bigger difference to rider confidence.
Mid-Drive vs Hub Motor: Final Verdict
There isn't a universal winner.
Choose a mid-drive motor if you:
Regularly climb very steep hills
Ride technical mountain trails
Want balanced weight distribution
Prefer a natural, performance-oriented riding feel
Don't mind additional drivetrain maintenance
Are comfortable paying more
Choose a hub motor if you:
Commute or ride recreationally
Mostly encounter flat to moderately hilly terrain
Want lower maintenance
Want better value for your budget
Prefer a mechanically simpler system
Want motor operation independent of the bicycle drivetrain
For many everyday riders, a quality geared hub motor offers the better balance of power, simplicity, reliability, and price. A properly designed 750W, high-torque hub-drive e-bike can handle far more than just flat city streets.
Mid-drives become particularly valuable when terrain gets genuinely demanding.
So instead of asking, "Which motor is better?", ask:
"Where will I actually ride this bike?"
If the answer is steep mountain trails and demanding climbs, look closely at mid-drives. If it's commuting, weekend rides, gravel roads, errands, and moderate hills, a good hub-drive e-bike—such as several models in Himiway's lineup—may give you everything you need without paying for complexity you won't use.