2402823_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2402823_en-US

2402823_en-US

S32K356 RTD Selection

We plan to use the S32K356, but found that only versions 7.0.0 and 7.0.1 are available, but the corresponding autosar...If using autosar R21, which version would you recommend?

wenming_0-1786093683425.png


Re: S32K356 RTD选择

I also tried SW32K3_S32M27x_RTD_R21-11_6.0.0_P05_D2510, but it failed many times. I suspect it's related to the S32Ds version. I've also tried 3.6.7. So, which version of S32D32 should I use?

wenming_0-1786106406261.png


Re: S32K356 RTD选择

Hello @wenming ,

You are right - even if the S32K356 is mentioned in the Supported Derivatives section of the  SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_ReleaseNotes.pdf , S32K356 project can't be created.

The RTD 6.0.0 P05 release notes state that this P05 release adds the S32DS/CT support for the S32K356 derivative. 

Best regards,

Pavel

Re: S32K356 RTD选择

Based on the description of version 6.0.0, it does not support S32K356.

wenming_0-1786103361744.png
Re: S32K356 RTD选择

Hello @wenming ,

S32K3 RTD versions 6.0.0 (AUTOSAR R21-11) is the recommended option for S32K356 with AUTOSAR R21.

Best regards,

Pavel

Re: S32K356 RTD选择

Hello @wenming ,

Thank you for the screenshot.

From the error message, this does not look like an S32DS version limitation. The error happens while S32DS is collecting/downloading the items to be installed, and the key message is:

Unexpected end of ZLIB input stream

The failed items are S32DS platform/debug related artifacts, for example:

com.nxp.s32ds.doc.platform.resources com.nxp.s32ds.lrc.gdb.arm64.linux.win32

This usually indicates that one of the artifacts was not downloaded completely or was corrupted during download/extraction. So the issue looks more like an update-site/download/cache problem than a direct RTD 7.0.1 versus S32DS 3.6.7 compatibility limitation.

Regarding the Release Note: the listed S32DS version should be understood as the baseline/tested S32DS version for that RTD release. However, S32DS is modular, and the RTD installation may still require related platform, tools, debugger, compiler, or documentation components to be updated or installed if they are missing or outdated in the current installation.

Please try the following:

  1. Restart S32DS and try the installation again.
  2. Make sure the network connection to the NXP update site is stable.
  3. If possible, use the official offline update-site ZIP/package instead of relying only on online download during installation.
  4. Check that the required GCC 10.2 toolchain is installed in S32DS.
  5. If the issue remains, please try a clean S32DS 3.6.x installation and then install the base RTD 7.0.1 package first before applying any additional patch/update package.

So based on the current screenshot, I would not conclude that RTD 7.0.1 cannot be used with S32DS 3.6.7. The current error points rather to an incomplete/corrupted download of required S32DS update artifacts.

For reference, I was able to install SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip successfully in S32DS 3.6.6. In my setup, I only had to additionally install the GCC 10.2 toolchain required by the S32K3 RTD package.
 

Best regards,

Pavel

Re: S32K356 RTD选择

I've upgraded my S32DS version to 3.6.10, which can install RTD 7.0.1 without requiring additional components. We'll use S32DS 3.6.10 + RTD 7.0.1 for development now. If autosar is needed later...If there's news of an update to version R21, please let me know. Thank you.

Re: S32K356 RTD选择

wenming_0-1786415389796.png

wenming_1-1786415468027.png


As shown in the image above, version 6.0.0 QLP01 also fails to install. Another issue is that the RTD release note states that only S32DS 3.6.2 is required for installation. Why is it prompting me to update components when I use version 3.6.7? This is related to the release...The note does not match; what could be the reason?

Re: S32K356 RTD选择

How do I resolve the S32DS version incompatibility issue? Why can't I install RTD7.0.1 in S32DS3.6.7, and it keeps prompting me to update?

wenming_0-1786513965538.png


Re: S32K356 RTD选择

Hello @wenming ,

Q1: How do I resolve the S32DS version incompatibility issue?

Could you please be more specific about the exact incompatibility message you see?
 

Q2: Why can't I install RTD7.0.1 in S32DS3.6.7, and it keeps prompting me to update?

The update prompt itself is not an error. S32DS may ask to update related platform/tool packages when the selected RTD package depends on newer or additional components.
 
Also, please make sure that the GCC 10.2 toolchain required by the S32K3 RTD package is installed in S32 Design Studio.
 

Best regards,

Pavel

Re: S32K356 RTD选择

wenming_0-1786523357428.png

This is an error message when installing RTD 7.0.1. Does it seem to be a version limitation? Also, the S32DS version described in the RTD release should, in principle, be ready to install without needing to update the S32DS components. If component updates are still required, it would be better to recommend the newer installation version, which would be easier to use.

タグ(1)
評価なし
バージョン履歴
最終更新日:
金曜日
更新者: