2402787_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2402787_en-US

2402787_en-US

Selection of FS2613 chip

The FS2613 series chips are quite powerful, and the values and timings of each power rail are editable. However, we don't have much time for software development and prefer not to implement OTP ourselves. Are there any models that are factory-configured to be compatible with the S32K358? For example, like the one shown in the image below?

Rio_Lee_0-1786090969347.png


Re: 关于FS2613芯片的选型

See attachment

Re: 关于FS2613芯片的选型

Okay, for the MFS2633AMDB2AD model, what are the output voltages of each of the following channels after power-on by default?

Where do VCORE, LDO1, LDO2, VREF, VBST, TRK1, and TRK2 originate?


Re: 关于FS2613芯片的选型

MFS2633AMDB2AD

Search | NXP Semiconductors

You can choose this one!

Re: 关于FS2613芯片的选型

The MFS2633AMDB2AD is discontinued. With the same specifications, I should replace it with the MFS2633HMDB2AD, right?

Re: 关于FS2613芯片的选型

Yes!

Re: 关于FS2613芯片的选型

Please submit a new ticket for new questions. Thank you!

Re: 关于FS2613芯片的选型

How are PIN.17 FCCU1 and PIN.18 FCCU2 used on this chip? What truth table do the input values of these two pins form, triggering different protection mechanisms of the chip?

タグ(1)
評価なし
バージョン履歴
最終更新日:
昨日
更新者: