manager:
Question:
(1) The FS32K144UAT0VLLT datasheet shows that it has 8 independent TIMEs, but I only see FTM0, FTM1, and FTM2. What else is also a TIME?
(2) Which TIME function of FS32K144UAT0VLLT has the Input capture function?
Thanks!
Hello, additional question:
1. In Table 47-1, FTM instances and features of S32K-RM Rev14.2, what is the parameter “Fault inputs”?
2. How many pages in the S32K-RM Rev14.2 manual show that each FTM has input capabilities?What about the capture function?
Thanks!
Hi
S32K-RM Rev14.2的Table 47-1. FTM instances and features 表格里S32K144只看到支持FTM0-FTM3. 你提到的应该是指每个FTM支持8 Channels通道。
都支持Input capture功能。 如果你要看FTM instances的功能区别也是看这个表格列出的功能才是某些FTM不支持的。
Best Regards,
Robin
A1. This refers to the number of external fault inputs supported. Taking the S32K144 as an example, Table 47-1 shows that it supports 4 inputs. You can see these 4 inputs, FTM0_FLT0\1\2\3, in the table on the left. Table 47-1. FTM instances and features Table 47-2. FTM signal descriptions.png
A2. The features supported by each FTM are usually not specifically listed. Refer to Table 47-5.The Channel Modes Selection configuration register can be used to implement the input capture mode mentioned in 47.5.5 Input Capture Mode.