2402455_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2402455_en-US

2402455_en-US

Problems encountered during IDE and RTD installation

Hello, I have installed S32DSIDE 3.6.6 software.

3859b5427f61973af225339173048fd.png

Then I installed the RTD package.

YangLuYao_0-1786007576122.png

However, the SDK cannot be found when creating a new application project, as shown in the image below.

YangLuYao_1-1786007624669.png

YangLuYao_2-1786007639499.png

This problem has been bothering me for a long time. I look forward to your reply. Thank you. My computer configuration is as follows:

YangLuYao_3-1786007691107.png

My computer has JDK 8 and JDK 17, and Python versions 13, 14, and 15 installed.

Re: 关于安装IDE和RTD遇到的问题

Thanks, I discovered this problem, and then I wanted to install gcc-10.2. I found a webpage about compilers.

YangLuYao_0-1786064846455.png

I didn't know which one to use, so I downloaded both of these EXE files to install.

YangLuYao_1-1786064901733.png

However, after installation, creating a new project in the S32DS software still did not show gcc-10.2.

YangLuYao_2-1786065074605.png

Then I tried to download it through the extension manager, but I kept getting errors and failing to download it successfully. Could you please guide me on what to do next? Thank you!

YangLuYao_3-1786065134265.png


Re: 关于安装IDE和RTD遇到的问题

Hello @YangLuYao,

I've translated your query, so please let me know if there are any misunderstandings.

Please try selecting NXP GCC 10.2 instead. S32K1 RTD does not support GCC 11.4 yet:

Julin_AragnM_0-1786049379556.png

Julin_AragnM_2-1786049434923.png

Best regards,
Julián

Re: 关于安装IDE和RTD遇到的问题I've solved the problem, thank you!Re: 关于安装IDE和RTD遇到的问题

Sorry, the past two days were the weekend, and this is the error message I reported this morning after trying to recreate the game.

YangLuYao_0-1786325441496.png


Re: 关于安装IDE和RTD遇到的问题

Hello @YangLuYao,

Sorry for the late reply. From the image, it seems you are trying to install NXP GCC 6.3.1 (build 1620), you should actually install v10.2 (build 1728):

Julin_AragnM_0-1786577752319.png

Julin_AragnM_1-1786577760152.png

If this still does not work, I guess you can try to install it externally: Installing software in S32 Design studio.

Things I would check:

  • Unstable network when installing.
  • Proxy / Firewall at your workplace.
  • Antivirus / Security checks.
  • Disk space.

Other than that, I'm not sure what could be the root cause. You could try re-installing S32DS and trying to install NXP GCC 10.2 again.

Best regards,
Julián

Tags (1)
No ratings
Version history
Last update:
4 hours ago
Updated by: