2402443_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2402443_en-US

2402443_en-US

Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hi,

I am currently integrating the AUTOSAR OS on the S32K144 MCU and have installed the S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0 DTM package.

After importing the OS module into EB tresos, I can only see the OSCounter container in the configuration editor. However, the OS User Manual describes additional configuration elements such as Tasks, ISRs, and other OS objects.

Could you please clarify:

  • Why are only OSCounter configurations visible in EB tresos?
  • Is there any additional plugin, license, or configuration step required to enable Task and ISR configuration?
  • What is the correct procedure for creating and configuring Tasks and ISRs for the S32K144 AUTOSAR OS?

Also I want to configure task, ISR and OS related configuration.
Any guidance or example project would be greatly appreciated.

Thanks

Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hi @Julián_AragónM ,

Thank you for your response.

Currently I'm using v29.0.0 version of EB Tresos

Devi_55_0-1786076176743.png

Could you please suggest the appropriate RTD version that is compatible with this EB tresos release?

Thank you for your support.


Best Regards,

Devi


Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hi @Devi_55,

SW32K14-OS401-RTM-1.0.0 b4.0.98 is legacy SW and no longer maintained. It is strongly recommended to transition to the newer RTDs (Real-Time Drivers for S32K1). For any further assistance or support, please reach out to your NXP representative. 

After installing SW32K14-OS401-RTM-1.0.0 b4.0.98 RTM, I can see all of the included ones below.

Julin_AragnM_0-1786054248282.png

The release notes for this SW package mentions EB Tresos v21.0.0, pelase confirm you are using this build.  

EB tresos Studio 21.0.0 b160607-0933

 Best regards,
Julián

Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hi @Devi_55,

Latest release of RTD for S32K1 (S32K1_S32M24x Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP07) uses EB Tresos v29.0.0:

Julin_AragnM_0-1786119367226.png

Best regards,
Julián

Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hello 

I apologize; this was an oversight by my part. 

RTD 3.0.0 QLP07 is the crypto release for the RTD drivers, QLP06 contains all of the base drivers (Adc, Can, Os, etc.):

Julin_AragnM_1-1786379905338.png

Best regards,
Julián


Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hello @Julián_AragónM ,

I have installed the S32K1_S32M24x Real-Time Drivers AUTOSAR R21-11 Version 3.0.0 QLP07 package, which is compatible with EB tresos v29.0.0. However, after reviewing the available plugins, I could not find several expected modules such as OS, ADC, Port, Dio, Spi, Can, Mcu, and other MCAL components.

Could you please suggest which RTD/AUTOSAR package I should use if I need access to the complete set of MCAL drivers along with an AUTOSAR OS?

If a different version of EB tresos is required for compatibility, I am willing to install and use the recommended version.

I would appreciate your guidance on the appropriate package and toolchain for the S32K144.

Devi_55_0-1786339741286.png

Thank you.
Best Regards,

Devi

Re: Unable to Configure Tasks and ISRs in AUTOSAR OS for S32K144

Hello @Julián_AragónM 

Thank you for your response.

I will verify this with the mentioned RTD version.



Thanks
Best Regards,
Devi 

Tags (1)
No ratings
Version history
Last update:
‎08-15-2026 02:34 AM
Updated by: