In the S32 Design Studio version 3.6.1, wanted to update the RTD version 7.0.0 but i could only update it to 5.0.0, its showing error when i try updating RTD version 6.0.0 and further.
i have installed the IDE 3.6.10 version, and tried to download the rtd version 7.0.1 but i couldnt, system network is connected properly, and it shows network issues only with this version and when i was working with the previous version 3.6.0 i didnt face any network issues. whenever i am opening the S32 IDE application the message box attached, pops up. If this is the case with changing network preferences, can you tell wat are the things to enable and disable in the settings?
and the RTD gets installed, and when i am trying to check with example project (DIO S32k344) it shows the above error as attached, in creating a new project i could not find any SDK options.
Hi @Rathidevi
First, we recommend updating your S32DS installation to version 3.6.10. There is no need to install it as a separate instance, as it can be installed as an update to your existing S32DS installation. Detailed instructions are available in the S32 Design Studio 3.6.10 RFP Installation Guide, which can be found on the same download page as the S32DS installer.
This update is recommended because RTD 7.0.1 was developed and validated using S32DS 3.6.4. To ensure compatibility and proper functionality, the IDE version should be the same as or newer than the version used for validation. Additionally, this requirement is noted in the Missing Requirements of the shared image.
Regarding the RTD 7.0.1 installation, we recommend first uninstalling the currently installed RTD version and then installing RTD 7.0.1. This helps avoid potential conflicts between different RTD versions.
BR, VaneB
Hi @Rathidevi
It seems that the toolchain required by the RTD is missing from your installation. Please install NXP GCC for Arm Release version 10.2 build 1728.
This should fix the problems with the examples and should also make RTD 7.0.1 available as an SDK option when creating a new project, as long as GCC 10.2 is selected as the project's toolchain.