2402414_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2402414_en-US

2402414_en-US

need alternative part number for MRF101AN.

I would appreciate if anyone could provide me the alternative part number for MRF101AN.?? And idea on availability for the same for next few years.

thank you!

Re: need alternative part number for MRF101AN.

**MRF101AN Status & Alternatives**

### Current Status
**MRF101AN** (NXP) is now in **End-of-Life / Last Time Buy**.

| Item | Details |
|----------------------------|--------------------------------------|
| **Lifecycle** | End of Life (EOL) / Last Time Buy |
| **Last Time Buy (LTB)** | **30 September 2026** |
| **Last Time Delivery (LTD)** | **30 September 2027** |
| **Reason** | NXP is ramping down the Radio Power product line |

After September 2026 you will no longer be able to place new orders with NXP. Remaining stock will be allocated on a first-come, first-served basis until the final shipment date in 2027.

---

### Closest Alternatives

| Part Number | Manufacturer | Key Differences | Compatibility | Recommendation |
|------------------|--------------|------------------------------------------|--------------------------------|--------------|
| **MRF101BN** | NXP | Mirror pin-out version of MRF101AN | Same package (TO-220), electrical performance almost identical | Best short-term option if pin-out can be flipped |
| **MRF300AN / MRF300BN** | NXP | 300 W version (higher power) | Different package (TO-247) | Only if you need higher power and can redesign |
| No official drop-in | — | NXP has **not** released a pin-compatible successor | — | — |

**Note**: NXP has not published an official pin-to-pin replacement for the MRF101AN. The **MRF101BN** is the closest device (same electrical characteristics, mirrored pin-out).

---

### Third-party / Competitive Alternatives (not pin-compatible)

These require board redesign but are still in active production:

- Ampleon BLF188XR / BLF189XRG (higher power, different package)
- STMicroelectronics STAC2932B or similar LDMOS devices
- Other 50 V LDMOS devices in the 100 W class from Infineon or MACOM (need matching for frequency and power)

---

### Availability Outlook (Next Few Years)

| Period | Availability Expectation |
|---------------------|----------------------------------------------|
| Now – Sep 2026 | Still orderable (Last Time Buy window) |
| Oct 2026 – Sep 2027 | Only remaining stock / residual shipments |
| After Sep 2027 | No new supply from NXP |

**Recommendation**:
1. Place a **Last Time Buy** as soon as possible if you still need this exact part.
2. Start evaluating **MRF101BN** (if pin-out change is acceptable) or begin a redesign to a currently active 50 V LDMOS device.
3. Contact : [email protected].

Would you like me to help compare specific electrical parameters of MRF101AN vs MRF101BN, or suggest possible redesign candidates based on your frequency and power requirements?

Tags (1)
No ratings
Version history
Last update:
a week ago
Updated by: