2402287_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2402287_en-US

2402287_en-US

Zephyr UAC2 → SAI reference on i.MX RT1020

Hi everyone,

I'm trying to get a USB-to-I2S audio pipeline working on the i.MX RT1020 using Zephyr's UAC2 asynchronous explicit feedback sample, but I'm running into issues with the NXP SAI (I2S) driver and eDMA.

Before I spend more time debugging DMAMUX and IRQ configuration, does anyone know of a working USB-to-I2S example for the RT10xx series using Zephyr?

I'm particularly looking for any reference project that implements a UAC2 to SAI audio path on Zephyr.

Thanks in advance!

Re: Zephyr UAC2 → SAI reference on i.MX RT1020

Hi @lpc73 ,

Thanks for your interest in NXP MIMXRT series!

There is currently no ready-made UAC2→SAI reference project for the RT10xx in upstream Zephyr. The building blocks are all supported on RT10xx: the SAI/I2S driver (nxp,mcux-i2s), eDMA, and the UAC2 class. DMAMUX routing is done via the devicetree properties nxp,tx-dma-channel / nxp,rx-dma-channel + pinctrl, not manually in C. The main piece you'll need to add is the feedback loop for the RT platform, and be sure to place DMA audio buffers in non-cacheable memory.

If Zephyr isn't mandatory, the MCUXpresso SDK's dev_audio_speaker + sai_edma_transfer are the most mature ready-to-use UAC2→SAI examples.

Best regards,
Gavin

タグ(1)
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: