2402128_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2402128_en-US

2402128_en-US

I need RTM 1.5 package for S32 Power architecture Design Studio Project

I am working on MPC5746 Target project using S32 Design Studio 2.1.

While importing i am facing issue w.r.t Project was created using SDK_S32_PA_15 which is not installed. If i try to forcefully convert the project, i am facing compilation errors in CPU.h files.

Please provide a compatible package.

image.pngimage.png

Re: I need RTM 1.5 package for S32 Power architecture Design Studio Project

Hello,

The SDK_S32_PA_15 is also known as S32 SDK 3.0.3. You can install this SDK into S32 Design Studio for PA v2.1 using the S32DS Extensions and Updates menu. This menu is located by: Help -> S32DS Extensions and Updates

 

petervlna_1-1786000019769.pngpetervlna_1-1786000019769.png

If this package is installed correctly, then you shouldn't receive this error message. 

Best regards,

Peter

标记 (1)
无评分
版本历史
最后更新:
3 周之前
更新人: