2402099_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2402099_en-US

2402099_en-US

S32K358 config tool dma has no DMA_IP_HW_INST_1

1. S32DS 3.6.10

2. chip S32K358

3. RTD: 7.0.1

problem: dma emux has no instance 1 ,just instance 0

Licunhao_0-1785922766915.png


this chip should have two instance of dma mux, but now the config tool just one.

I want to use LPUart4 DMA,but it is in mux1.

Someone give me a help.

Re: S32K358 config tool dma has no DMA_IP_HW_INST_1

Hi,

There is a single DMA module with 32 DMA channels and two DMAMUX instances. Each DMAMUX instance provides 16 channels and is mapped to half of the DMA channels.

PetrS_0-1785931235713.png

As the LPUART4 TX request is routed to DMAMUX1, you need to use DMA channels 16-31.
 
The DMAMUX configuration is handled in the RM component, so please add the RM component to the project and configure it accordingly.

PetrS_1-1785931415785.pngPetrS_2-1785931424284.png

BR, Petr

タグ(1)
評価なし
バージョン履歴
最終更新日:
1週間前
更新者: