2401781_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2401781_en-US

2401781_en-US

CodeWarrior for LA1224 plugin

Hello, 

I am currently In the middle of evaluating LA1224-RDB and I have some questions regarding the software environment. As I understand I can have a Linux app running on the existing NxP image on LX2160A for evaluation purposes. Furthermore I suppose LA1224 is running baremetal with freertos. I saw that I can have firmware for LA1224 in a Linux directory on the LX2160A. Is this given from NxP? What does it support? I suppose that if I want to develop something further than the given firmware I have to get a codewarrior license and TAP.

I have downloaded CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe however the LP1224 is not available. After searching the NxP site I read that I need an extra toolchain on top of CW_ARMv8. What is the full url to download the add on?  I read CodeWarrior for LA1224 and only a partial url is given "com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip"

Any further information on how to work on those processors is welcome.

Kind Regards
N. Alexopoulos

Re: CodeWarrior for LA1224 plugin

Please download pack com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from the following link.

https://support.nxp.com/s/case/500Te00000eF7lOIAS/community-codewarrior-for-la1224-plugin?language=e...

Please prepare a clean installation environment. Please install CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe first. Then open CodeWarrior IDE in a new worksapce path. Then install the service pack com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from Help->Install New Software->Add->Archive in CodeWarrior IDE.

标记 (1)
无评分
版本历史
最后更新:
2 周之前
更新人: