2401506_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2401506_en-US

2401506_en-US

i.MXRT685S: Boot from external flash via HS SPI bus

I have an external SPI NOR flash device wired to the HS SPI bus interface (Flexcomm 14) on a RT685s. I want to boot from this flash device; however, I've read that the only master boot options are a FlexSPI boot, SD boot, and eMMC boot. Is it possible to boot from this external flash using the high-speed SPI bus (Flexcomm 14)? If so, what are the requirements/setup steps I must follow to execute this?

Re: i.MXRT685S: Boot from external flash via HS SPI bus

Here below is some application notes for reference for NOR boot 

AN12751 How to Enable Recovery Boot from QSPI Flash

AN12773 How to Enable Master Boot from Serial NOR Flash

Re: i.MXRT685S: Boot from external flash via HS SPI bus

Hi @lgibarra9,

It is not possible to boot from an external SPI NOR Flash using the High-Speed SPI bus from FC14. This bus can be used (besides run-time SPI communication) to download an image when the MCU is in ISP mode. But for normal boot operation from an external flash, the High-Speed SPI bus is not an option, so your SPI NOR flash should instead be connected to the FlexSPI bus.

BR,
Edwin.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-04-2026 02:31 AM
更新者: