2400668_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2400668_en-US

2400668_en-US

Regarding FEE initialization time

Hi, NXP expert, I have an issue with the S32K312 feed initialization time and would like to consult about it. The details are as follows:
I configured two fee storage clustergroups, one primary and one standby. The standby is a backup of the primary. A total of 19 blocks were configured, and the blocks are stored in both the primary and standby. The software version is Mcal RTD4.0.0 HF02, and Burst mode is enabled.

Chenxu1_0-1785460201957.pngChenxu1_0-1785460201957.png

Test method:

Upon power-up, the initialization time is printed (after calling Mem_43_INFLS_Initt(), MemAcc_Initt(), and Fee_Init(), wait for the Fee_GetStatus() interface to return MEMIF_IDLE), and all blocks are written with data once.

The test results are as follows:

Number of power-ups

Initialization time (ms)

illustrate

1

8


2

15


3

twenty three


4

40


5

48


6

57


7

65


8

74


9

82


10

90


11

99


12

107


13

115


14

124


15

133


16

141


17

149


18

158


19

166


20

175


twenty one

183


twenty two

192


twenty three

200


twenty four

209


25

217


26

226


27

234


28

8

Cluster paging


Based on the above tests, we found that the time for each increment changes very quickly. Therefore, we would like to inquire whether there is a formula for calculating the initial time and whether it can be optimized.

Re: 关于FEE初始化时间

Hi @Chenxu1 


There is no formula provided by the FEE driver documentation to calculate the initialization time. The initialization time depends on the actual state of the FEE storage, such as the amount of stored data, number of records, and whether any cluster recovery or swap is required. The main configuration parameter that can improve initialization performance is FeeDataBufferSize, as a larger buffer allows more data to be processed per Fls_MainFunction cycle. See please Fee user manual for details. For a realistic estimate, the initialization time should be measured on the target configuration after prolonged FEE usage and multiple write cycles.


Regards,

Lukas

Re: 关于FEE初始化时间

Yes, this has been discussed here several times. For example:

https://community.nxp.com/t5/S32K/S32K312-FEE-FLS-INIT-time/m-p/2024041

Regards,

Lukas


Re: 关于FEE初始化时间

Hi,
Currently, writing 16 bytes causes the next initialization to take 2ms longer. At this point, there's no page switching involved—just reinitializing and reading 16 bytes again, which adds 2ms. Is this normal?

Tags (1)
No ratings
Version history
Last update:
‎08-04-2026 02:31 AM
Updated by: