2399669_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2399669_en-US

2399669_en-US

Issue with iMXRT1176DVMAA + Macronix MX25U51245G 54 flash

Hi, working with a custom board and we need to change a functional flash for Macronix MX25U51245G 54 because of supply chain issues. I've had issues with what I suspect is the SFDP discovery using the bootloader ROM API.

  • Custom PCBA using MIMXRT1176DVMAA
  • Changed flash device from Winbond W25Q512NWEIQ to Macronix MX25U51245G 54
  • Using FlexSPI1
  • 1V8 power
  • Signal integrity within specifications

Here is the schematics connection:

achampoux_0-1785249761617.pngachampoux_0-1785249761617.png

achampoux_1-1785249804702.pngachampoux_1-1785249804702.png

By default, with the new flash, I can't perform write/erase operations properly using either the serial downloader or LinkServer. Reading the flash however seems to work.

I was able to properly write/read/erase on the new flash by modifying example project evkbmimxrt1170_flexspi_nor_polling_transfer_cm7 from SDK 25.12.00 to run on RAM (TCM) and changing only tcustomLUT in board/hardware_init.c. Here is the LUT in question:

const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x03,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04,
            kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0B,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] =
        FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x0A,
            kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xEB,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] =
        FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x0A,
            kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04
        ),
    [4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] =
        FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06,
            kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x20,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x02,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE + 1] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04,
            kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x38,
            kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x20
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x04,
            kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READID] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F,
            kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x03
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
        FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01,
            kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x02
        ),
	[4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG] =
		FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05,
            kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x01
        ),
    [4 * NOR_CMD_LUT_SEQ_IDX_ERASECHIP] =
        FLEXSPI_LUT_SEQ(
            kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xC7,
            kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0
        ),
};

Are there known issues with this flash device and the bootloader API or SFDP discovery?

Re: Issue with iMXRT1176DVMAA + Macronix MX25U51245G 54 flash

Hi @achampoux ,

Thanks for your interest in NXP MIMXRT series!

I checked the datasheet for the Flash chip you're using (MX25U51245G 54) and found that it appears to have some unique features.

Most importantly: 4-Byte Address Mode permanent 

I suspect that the LUT automatically generated by flashloader may not be using the 4-byte address mode. I recommend that you check this by looking at the fsl_romapi project in SDK. 

ROM_FLEXSPI_NorFlash_GetConfig(instance, &norConfig, &option);
 
Next, retrieve norConfig and check its value. If this is indeed the issue, you’ll need to use a custom FCB header directly in serial download mode instead of the one generated by the tool. When downloading via the debugger, you’ll need to use a custom download algorithm.
 
Best regards,
Gavin
Tags (1)
No ratings
Version history
Last update:
a month ago
Updated by: