2399642_ja-JP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2399642_ja-JP

2399642_ja-JP

IMX93はmcimx93evk_ethosu_apps(SDK2.14)でエルフをロードできません

SDK2.14のデモを試してみたいです:
mcimx93evk_ethosu_apps
エルフの後に 。このエルフをm33にロードします。
失敗した:
remoteproc remoteproc0: 登録されたカーブアウトがDAリクエストに合いません
[ 236.970879] rproc-virtio: rproc-virtio.1.車載のプローブエラー-12で失敗
[ 236.984471] リモートプロック リモートプロック0: 登録されたカブアウトがこの申請に合致しません
[ 236.992036] Rproc-virtio: rproc-virtio.2.車載のプローブがエラー-12で失敗

何が起こったのか分からない。

Re: imx93 cannot load elf in mcimx93evk_ethosu_apps (sdk2.14)

こんにちは、@bighero77 さん

NXPサポートまでご連絡いただきありがとうございます。

READMEファイルによると、あなたのユースCASEに必要なアプリケーションはethosu_apps_rpmsgであり、ethosu_appsではありません。

README抜粋:

4. Test process
---------------
4.1 Example ethosu_apps_rpmsg is built as .out or .elf and installed in rootfs. In Linux command line,
    user can run the following command to do inference for the model.
    #./inference_runner -d /dev/ethosu0 -n mobilenet_v1_1.0_224_pb_int8_vela.tflite -i stopwatch.bmp -l labels.txt -o output_data_detection -t 1080000000

    When the examples runs, the log and inference result would be seen on the terminal as below.

    Send Ping
    Send version request
    Send capabilities request
    Capabilities:
            version_status:1
            version:{ major=0, minor=0, patch=0 }
            product:{ major=6, minor=0, patch=0 }
            architecture:{ major=1, minor=0, patch=6 }
            driver:{ major=0, minor=16, patch=0 }
            macs_per_cc:8
            cmd_stream_version:0
            custom_dma:false
    Create network
    Create inference
    Wait for inferences
    Inference status: success

    Detected: jinrikisha, confidence:70
    Detected: horse cart, confidence:70
    Detected: academic gown, confidence:70
    Detected: howler monkey, confidence:70

    For other demos, such as face recognition, please refer to the user manual.

4.2 Example ethous_apps is built as .bin. In U-Boot prompt, user can run the following command to do
    inference for the conv2d op model.
    u-boot=> tftp 0x80000000 ethosu_apps.bin;cp.b 0x80000000 0x201e0000 0x20000;bootaux 0x201e0000 0

    When the example runs, the log and inference result would be seen on the terminal as below.

    Initialize Arm Ethos-U
    Inference status: success

ドキュメントによると、もしLinuxから/dev/ethosu0を使って推論を実行するのが目標なら、このアプリethosu_apps_rpmsg正しいです。

よろしくお願いします、
アレハンドロ・ガルシア

标记 (1)
无评分
版本历史
最后更新:
1 个月之前
更新人: