2399440_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2399440_en-US

2399440_en-US

Windows 10/11 IoT Enterprise support and installation procedure for IMX95LPD5EVK-19

Hello NXP Team,

We have an NXP i.MX95 19 mm × 19 mm evaluation kit with the following details:

  • EVK: IMX95LPD5EVK-19

  • Baseboard marking: IMX95LPD5BB-19 REV B

  • Intended installation target: Onboard eMMC

We would like to install Windows 10/11 IoT Enterprise ARM64, preferably Windows 10/11 IoT Enterprise LTSC 2024, on this board.

Could you please confirm whether Windows 11 IoT Enterprise is supported on the IMX95LPD5EVK-19?

If supported, please share the official BSP, required software packages, and the complete installation or flashing procedure that we can use as a reference to install Windows onto the onboard eMMC.

We are specifically looking for an official, board-validated guide for the IMX95LPD5EVK-19.

Thank you.

Regards,
Jhasim

Windows 10 IoT EnterpriseRe: Windows 10/11 IoT Enterprise support and installation procedure for IMX95LPD5EVK-19Thank you @yipingwang for the confirmation.

Understood that there is currently no publicly released or officially supported Windows 10/11 IoT Enterprise BSP or board-validated installation procedure for the IMX95LPD5EVK-19.
We will monitor the NXP Windows IoT BSP release page for any future i.MX95 support.

Thank you.
Re: Windows 10/11 IoT Enterprise support and installation procedure for IMX95LPD5EVK-19

At present, we are unable to locate any publicly released or officially documented Windows 10/11 IoT Enterprise BSP for the IMX95LPD5EVK-19. The current NXP Windows IoT support pages and Microsoft Windows IoT support matrices list support for i.MX8 family devices and i.MX93 EVK, but do not list i.MX95 EVK. Therefore, we cannot provide an official Windows installation procedure, BSP package, or board-validated flashing guide for IMX95LPD5EVK-19 at this time. If Windows support for i.MX95 becomes available through NXP, it would be expected to be published through the NXP Windows IoT BSP release page and accompanying release notes.

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/windows-10-11-iot-...

タグ(1)
評価なし
バージョン履歴
最終更新日:
1ヶ月前
更新者: