2399434_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2399434_en-US

2399434_en-US

Flashing Issue on IMX95EVK's M7 core

Hello,


I am trying to run an M7 application on IMX95LPD5EVK-19 following AN14748, but I cannot flash flash.bin with UUU. The board is detected briefly, then SDPS boot fails immediately.

Hardware: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.)
Boot switch (SW7[1:4]): 1001 (Serial Download)
Target: eMMC
Host: Ubuntu Linux
UUU: libuuu_1.5.243-0-g230f1b1

SDKs tried (MCUXpresso SDK Builder):

  • SDK_26.06.00_IMX95LPD5EVK-19
  • SDK_2.15.000_IMX95LPD5EVK-19

Both produce the same result.

Command:

cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk
sudo uuu -b emmc flash.bin
 

Error:

Success 0 Failure 1
1:2-E3C50910 1/ 1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin
 

Steps followed (per AN14748):

  1. Set SW7 = 1001 with board powered off
  2. Connect USB to host
  3. Run sudo uuu -b emmc flash.bin
  4. Power-cycle board
  5. Fails at SDPS boot every time

Please share the steps to flash and the BSP version supported for M7 core for this version of the board.

Re: Flashing Issue on IMX95EVK's M7 core

Hello,

The latest supported BSP for A1 revision is Linux 6.12.20.

Also, you could try to build the the whole binary from scratch (Uboot+SPL+ATF+Firmware+M-SDK).

#### Download and extract ARM GCC toolchain ####
$ sudo tar -xvJf arm-gnu-toolchain-14.3.rel1-x86_64-aarch64-none-linux-gnu.tar.xz -C /opt
$ sudo tar -xvf arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi.tar.xz -C /opt
$ sudo tar -xvf arm-gnu-toolchain-14.2.rel1-x86_64-arm-none-eabi.tar.xz -C /opt

#### Get NXP code necessary for the i.MX95 #### In your case be careful with the latest supported BSP version. 
$ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.18.2-1.0.0
$ git clone https://github.com/nxp-imx/imx-atf -b lf-6.18.2-1.0.0
$ git clone https://github.com/nxp-imx/imx-sm -b lf-6.18.2-1.0.0
$ git clone https://github.com/nxp-imx/imx-oei -b lf-6.18.2-1.0.0
$ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.18.2-1.0.0
$ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-ele-imx-2.0.5-29313e0.bin
$ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.31-4fa5b46.bin

#### Build Uboot ####
$ cd uboot-imx
$ make -j $(nproc --all) clean
$ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-14.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- imx95_19x19_evk_defconfig
$ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-14.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-

#### Build ATF ####
$ cd ..
$ cd imx-atf
$ make -j $(nproc --all) PLAT=imx95 bl31 CROSS_COMPILE=/opt/arm-gnu-toolchain-14.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-

#### Build SM ####
$ cd ..
$ cd imx-sm
$ make -j $(nproc --all) TOOLS=/opt/ config=mx95evk cfg (optional if the associated mx95evk.cfg file has been changed)
$ make -j $(nproc --all) TOOLS=/opt/ config=mx95evk all (Linux+M7)
$ make -j $(nproc --all) TOOLS=/opt/ config=mx95alt all (config for MCUXpresso testing)

#### Build OEI ####
$ cd ..
$ cd imx-sm
$ make -j $(nproc --all) TOOLS=/opt/ board=mx95lp5 oei=ddr DEBUG=1
$ make -j $(nproc --all) TOOLS=/opt/ board=mx95lp5 oei=tcm DEBUG=1 (for i.MX 95 A1 only)

#### Extract Firmware ####
$ cd ..
$ chmod +x firmware-ele-imx-2.0.5-29313e0.bin
$ ./firmware-ele-imx-2.0.5-29313e0.bin --auto-accept
$ chmod +x firmware-imx-8.31-4fa5b46.bin
$ ./firmware-imx-8.31-4fa5b46.bin --auto-accept

#### M7 SDK compilation ####
$ unzip SDK_25_12_00_IMX95LPD5EVK-19.zip
$ python3 -m venv .venv
$ source .venv/bin/activate
$ export ARMGCC_DIR=/opt/arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-eabi
$ pip install west
$ west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b imx95lpd5evk19 -Dcore_id=cm7 #### For ITCM ####
$ west build -p always examples/demo_apps/hello_world --toolchain armgcc --config ddr_release -b imx95lpd5evk19 -Dcore_id=cm7 #### For DDR ####
$ exit (this will close the terminal so re-open the terminal)

#### Copy the resulting binaries to imx-mkimage ####
$ cd imx-mkimage
$ cp ../uboot-imx/u-boot.bin ./iMX95
$ cp ../uboot-imx/spl/u-boot-spl.bin ./iMX95
$ cp ../imx-atf/bl31.bin ./iMX95
$ cp ../imx-oei/oei-m33-ddr.bin ./iMX95
$ cp ../imx-sm/m33_image.bin ./iMX95
$ cp ../mcuxsdk/build/hello_world_cm7.bin ./iMX95/m7_image.bin
$ cp ../firmware-imx-8.31-4fa5b46/firmware/ddr/synopsys/lpddr5_dmem_qb_v202409.bin ./iMX95
$ cp ../firmware-imx-8.31-4fa5b46/firmware/ddr/synopsys/lpddr5_dmem_v202409.bin ./iMX95
$ cp ../firmware-imx-8.31-4fa5b46/firmware/ddr/synopsys/lpddr5_imem_qb_v202409.bin ./iMX95
$ cp ../firmware-imx-8.31-4fa5b46/firmware/ddr/synopsys/lpddr5_imem_v202409.bin ./iMX95
$ cp ../firmware-ele-imx-2.0.5-29313e0/mx95b0-ahab-container.img ./iMX95
$ make SOC=iMX95 OEI=YES flash_all

You may use the resulting binary to flash your EVK, we tested this in standalone mode and it is working correctly.

Best regards.

Re: Flashing Issue on IMX95EVK's M7 core

db16122_0-1785222133220.pngdb16122_0-1785222133220.png

if boot from EMMC, SW7-3 should be 1 according to Quick Start Guide
IMX95LPD5EVK-19

Re: Flashing Issue on IMX95EVK's M7 core

Hello,

Thank you for the update.

Please try with sudo command.

Best regards.

Re: Flashing Issue on IMX95EVK's M7 core

Hi @JorgeCas 
I have followed the exact steps given by you.

But there is a same flashing error. It goes till 60% and failed after sometime.
Can you please check the below screenshots and let me know whether the commands are right.

Thanks,

Gaurav


Screenshot from 2026-07-31 17-31-12.pngScreenshot from 2026-07-31 17-31-12.pngScreenshot from 2026-07-31 17-31-20.pngScreenshot from 2026-07-31 17-31-20.png

Re: Flashing Issue on IMX95EVK's M7 core

why there is usb error no device?does it happen at 60% booting process?

Re: Flashing Issue on IMX95EVK's M7 core

Hello,

I found a new resource that suggest use Linux 6.12.3_1.0.0/SDK25.03.00 for A1 silicon revision, please try again with this software versions.

What do you see in Cortex-A console when you see the error log?

Best regards.

Re: Flashing Issue on IMX95EVK's M7 core

And I am working on the lf-6.12 version for all the repos. Switch position for download mode is "1 0 0 1"

Can you please also confirm the supported version of M7 SDK?

Re: Flashing Issue on IMX95EVK's M7 core

can this issue be reproduced as failed at 60% process all the time?

Re: Flashing Issue on IMX95EVK's M7 core

Hi @db16122 ,

Thanks for replying.

Yes while flashing the firmware it is getting failed gets stuck at 60% for sometime and getting failed after that. 


Thanks,

Gaurav C.

Re: Flashing Issue on IMX95EVK's M7 core

Hi @JorgeCas ,

I have tried with sudo command as well but there is no change and it is still failing.

Please check the below screenshot.


Thanks,

Gaurav C.

Screenshot from 2026-08-03 09-14-48.pngScreenshot from 2026-08-03 09-14-48.png

Re: Flashing Issue on IMX95EVK's M7 core

Yes, it is happening everytime.

Re: Flashing Issue on IMX95EVK's M7 core

Hi @JorgeCas 

I have tried with SDK 25.03 and i am only getting some failure logs on /dev/ttyUSB3 while flashing the binary.

I have also copied the file like below.

cp ../firmware-ele-imx-2.0.5-29313e0/mx95b0-ahab-container.img ./iMX95

Do you think there exists a file for mx95a1-ahab-container.img as well?

Please also go through the screenshot, it is showing the SOC IMX95(A0) while I am having A1 revision.

Thanks

Gaurav


Screenshot from 2026-08-05 17-49-46.pngScreenshot from 2026-08-05 17-49-46.png

Re: Flashing Issue on IMX95EVK's M7 core

Hi @JorgeCas 

I am able to resolve this issue using document AN14748 and SDK25.03.00 

Thanks for your suggestions and valuable time.


Thanks,

Gaurav

タグ(1)
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: