2398744_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2398744_en-US

2398744_en-US

S32DS 3.6.5 upgrade to 3.6.8 - missing "move to line" in debug context menu

I had installed S32DS 3.6.5 and using it happily. In my debug sessions I could right-click on a code line and choose "Move To Line" to force running from that line. After upgrading to 3.6.8 via the "Check for updates" the right-click context menu in the "S32DS Debug" context shows the "S32DS C/C++" menu instead.

How do I change the right-click to show the correct context menu?

I am currently having to show the Disassembly view and scrolling to the 1st assembler instruction of my C line. In the Disassembly window I get the correct "Move To Line", "Run To Line" etc. context menu.

I cannot run the S32DS 3.6.8 standalone installer due to IT restrictions at work. It would hang during preparing for installation. I think IT blocks some Java stuff. However, the "Check for updates" method worked (or did it?).

Thanks

Darren

Re: S32DS 3.6.5 upgrade to 3.6.8 - missing "move to line" in debug context menu

Hi @DarrenD 

I have checked S32 Design Studio 3.6.10, which is the latest S32DS release available, and I can confirm that the "Move to Line" option is still present. As shown in the image below, the feature remains available and can still be used to navigate directly to a specific line within the editor.

VaneB_0-1785185870489.pngVaneB_0-1785185870489.png


BR, VaneB

Re: S32DS 3.6.5 upgrade to 3.6.8 - missing "move to line" in debug context menu

I'm not sure what happened with my upgrade of 3.6.5 to 3.6.8 via the IDE then.

However, I have since found out that standalone installs of 3.6.8 (into C:\NXP\S32D.3.6.8) and then 3.6.10 (into C:\NXP\S32D.3.6.10) both worked. Each took about 3 hours to install possibly due to IT scanning every single file. In both cases the "Move To Line" option is there so I am happy again.

We use v10.2 of the compiler so I just copied the "C:\NXP\S32DS.3.6.5\S32DS\build_tools\gcc_v10.2" folder to "C:\NXP\S32DS.3.6.10\S32DS\build_tools\" and now my compilations work in 3.6.10.

Thanks

Tags (1)
No ratings
Version history
Last update:
a month ago
Updated by: