Dear Everyone,
I would like to ask for any possible reason why does our flash driver fail in one specific situation.
We use custom board with IMXRT1176, our board is based on Embedded Artists carrier board for that MCU. In our project there are two partitions in flash, 0x30100000 and 0x30200000. We use MCU-Link and Linkserver to flash binaries. Binaries are signed with --confirmed in this case. We have a FLASH remap functionality enabled so no swap is performed.
We observe two situations:
1. If there is a bootloader in flash and an image in partition 1, everything works as expected.
2. Once we complete the OTA upgrade and MCUboot boots new image from a second partition, we can no longer write to FLASH partiton 1 as we get an error from linkserver:
=================================================
Nc: Opening flash driver MIMXRT1170_SFDP_QSPI.cfx (already resident)
Nc: Sending VECTRESET to run flash driver
Nc: Flash variant 'iMXRT1170_SFDP_FlexSPI1_A_QSPI May 15 2026 18:32:39' detected (16MB = 256*64K at 0x30000000)
Pb: 1 of 1 ( 0) Writing sectors 16-31 at 0x30100000 with 1048576 bytes
Ps: ( 0) at 30100000: 0 bytes - 0/1048576
Ec: op ProgramPage (0x30100000, 0x20002830, 0x4000) status 0x1 - driver reported driver error - EXTSPIJ driver rc 1 - Operation failed
Ec: op ProgramPage (0x30100000, 0x20002830, 0x4000) status 0x1 - driver reported driver error - EXTSPIJ driver rc 1 - Operation failed
Note that I have erased the first partition with erase-range. I also can confirm that when our firmware does it with flash driver it works as expected. It fails only when i try to do it with the linkserver manually
===================================================
Q1. Is there any obvious reason for it? Should we always erase partition 2 or both paritions?
Q2. If we have binary built for slot1, does this binary work when we attach to the core which runs with image in partition 2? Does Flash remap make it work?
Thanks in advance for any help,
Best Regards!
Jakub
Hello Gavin, thank you very much for your response! You really helped me to understand these concepts.
If it's possible, could you please help me figure out one more thing?
This is partition info i get after OTA:
===========
Image 0; name APP; state Permanent:
Slot 0 APP_PRIMARY; offset 0x100000; size 0x100000 (1048576):
< size="" 821444="">
SHA256 of image payload: C825709456C098E38090...
log_addr 0x30100000 remaps to 0x30200000
Slot 1 APP_SECONDARY; offset 0x200000; size 0x100000 (1048576):
< size="" 821444="">
SHA256 of image payload: EBFCCC0D3E970230E404...
log_addr 0x30200000 remaps to 0x30200000
*ACTIVE*
===============
Then I run this script to clear slot0
LinkServer.exe flash MIMXRT1176xxxxx:MIMXRT1170-EVKB erase-range 0x30100000 0x100000
According to what you said, i expected to erase slot1 because remap overlay is active. However that's not the case. What i got after power reset is:
=========
Flash REMAP_OVERLAY active.
Image 0; name APP; state None:
Slot 0 APP_PRIMARY; offset 0x100000; size 0x100000 (1048576):
Slot 1 APP_SECONDARY; offset 0x200000; size 0x100000 (1048576):
< size="" 821444="">
SHA256 of image payload: EBFCCC0D3E970230E404...
log_addr 0x30200000 remaps to 0x30200000
*ACTIVE*=========
I still can't write anything to slot0 which is unexpected. Is it possible that erase bypasses the logical mapping of remap but load doesn't?
Hi @jslota13245 ,
Thanks for your interest in NXP MIMXRT series!
Based on the information you provided, I believe the following reasons should be considered. The failure is caused by the FlexSPI remap still being enabled after OTA. When MCUboot boots slot1 (partition2) via remap, it leaves remap on into the application. LinkServer's .cfx flash driver programs through the AHB logical address, so the remap silently redirects your write to 0x30100000 (partition1) to physical 0x30200000 (partition2) — which already holds the confirmed image and is not blank. NOR flash cannot overwrite it.
Your earlier erase-range 0x30100000 actually erased partition2 for the same reason. Your own firmware works because it programs via FlexSPI IP command mode with explicit physical offsets, bypassing the remap. Note: VECTRESET / debugger attach do not clear the remap — only a POR or an explicit register write does.
Q1: Which partition to erase?
The key is to disable remap first, not just erasing partitions. Recommended:
Q2: Will a slot1 binary work when attached to a core running the partition2 image?
The image should be linked once for the primary slot (0x30100000); the same binary runs from either slot via remap — no separate slot1 build is needed. When you attach for debug, remap keeps logical addresses consistent, so code reads/breakpoints work fine. However, the same remap changes the physical target when writing flash, so you must disable remap before programming slot0 with LinkServer.
Best regards,
Gavin
@Gavin_Jia
Dear Gavin,
could you please have a look at my comment to your response and let me if we missed something?
Thanks a lot for your help!
Best Regards,
Jakub
Hi @jslota13245 ,
Apologies for missing your previous message.
Unfortunately, once an answer is marked as accepted, the system automatically considers the issue resolved, and I no longer receive updates on the case. Please accept my sincere apologies for the oversight.
I will try to reproduce the issue on my side. Please allow me some time to investigate, and I will keep you informed of any findings or progress.
Thank you in advance for your patience and understanding.
Best regards,
Gavin
Hi @jslota13245 ,
Hope you are doing well!
I continued to look into the matter further, and this post offers some preliminary conclusions: https://www.cnblogs.com/henjay724/p/13538105.html
Erase and program are not affected by the remap. Both go through FlexSPI IP commands on physical addresses, so your erase-range 0x30100000 really did erase the physical slot0 — that is why slot0 shows No Image Found and slot1 is intact. My earlier wording about erase hitting slot1 was not accurate, sorry for that. The reason the write still fails is the read-back verify, not the write itself.
I believe the simplest solution is still to disable the remap function before flashing the image. Alternatively, after flashing, use an IP command to read back the data from memory; if it matches the data that was written, this proves that the failure was merely due to the AHB checksum being cheated.
In addition, the official statement supports the earlier speculation: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/examples/ota_examples/_doc/flash_remap_readme.html#mc...