The EdgeLock Enclave (ELE) / System Manager firmware fails to initialize during boot:
[ 0.182931] fsl-se-fw se-fw2: Command Id[23], Response Failure = 0x29
[ 0.182942] fsl-se-fw se-fw2: Failed to initialize ele fw.
Because ELE fails to initialize:
The Mali GPU (4d900000.gpu) power domain stays off, triggering an ARM64 SError Interrupt kernel panic when Linux probes the GPU.
Disabling the GPU node allows boot to proceed further, but USDHC storage (mmc0 and mmc1) fails initialization with error -5, preventing Linux from mounting the root filesystem (/dev/mmcblk*p2).
Using "Reinstall system" does not resolve this issue. Could an admin please reflash the primary bootloader/ELE firmware on unit FRDM-IMX95-1?
Hello,
Could you please share more about your testing SW/HW setup?
If you are using a custom image please share the changes.
Also, please try to re-flash the board.
Best regards.