2397882_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2397882_en-US

2397882_en-US

How to test Sideband ECC error injection on i.MX 8QuadXPlus / i.MX 8DualXPlus?

Hello NXP team,

I am testing the DDR Sideband ECC functionality on an i.MX 8QuadXPlus / i.MX 8DualXPlus platform with a 40-bit DDR3L interface (32-bit data + 8-bit ECC).

According to AN13566, Inline ECC errors can be injected by unlocking the ECC parity region through ECC_REGION_PARITY_LOCK and modifying the ECC parity bits. However, I could not find a detailed error-injection or validation procedure for Sideband ECC.

AN13566 mentions that Sideband ECC uses an additional ECC byte and that the controller checks this byte during DDR reads. It also mentions that Sideband ECC supports an automatic scrub RMW operation after detecting a correctable single-bit error.

Could you please clarify the recommended method to test Sideband ECC?

  1. Is there a hardware error-injection or data-poisoning register for Sideband ECC?
  2. How can software inject a single-bit correctable error?
  3. How can software inject a double-bit uncorrectable error?
  4. Which ECC status registers and interrupt signals should be checked?
  5. How can we verify that the Sideband ECC scrub operation has corrected and written back the data?
  6. Is there any example code, test procedure, or DDR controller register sequence available?

Our configuration is:

  • SoC: i.MX 8QuadXPlus / i.MX 8DualXPlus
  • DDR type: DDR3L
  • DDR interface: 40-bit, 32-bit data + 8-bit ECC

Thanks.

Re: How to test Sideband ECC error injection on i.MX 8QuadXPlus / i.MX 8DualXPlus?

Hi @kkfly 

You can refer to the description of the ECC register in the IMX8DXL RM documentation.

https://www.nxp.com/products/iMX8XLite

In particular, the ECC Configuration Register 0 (ECCCFG0) and ECC Configuration Register 1 (ECCCFG1) registers.

pengyong_zhang_0-1784880352446.png


B.R

Re: How to test Sideband ECC error injection on i.MX 8QuadXPlus / i.MX 8DualXPlus?

The doc says 'NOTE: ECC data poisoning is not supported in this SoC. Please ensure this bit setting is 0.' So does that mean the IMX8DXL and IMX8QXP don't support ECC error injection?

Tags (1)
No ratings
Version history
Last update:
3 weeks ago
Updated by: