2397597_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2397597_en-US

2397597_en-US

IW611 RU setup

I would like some advice on how to set up the RU.

For the RF test, the technical staff is conducting the test by referring to Chapter 12 of the manual “UM11749” for RU setup. However, when we edited the configuration file “TF_Config_20MHz.txt” and loaded it based on the example in Chapter 12.6, the output waveform resembled an unmodulated signal, and we were unable to confirm the expected waveform.

Since a waveform is being output, we believe the file was loaded correctly.

The configuration file is described as follows.

===================================================================

FRAME_CTRL_TYPE=1 \\IEEE_TYPE_CONTROL

FRAME_CTRL_SUBTYPE=2 \\TRIGGER


\\configure Duration field

\\ Max Duration time

FRAME_DURATION=5484 \\0x156C


\\configure commoninfo field of trigger frame

\\ HE_trigger_frame.TrigCommonField.TriggerType = BASIC_TRIGGER;

\\ HE_trigger_frame.TrigCommonField.UlLen = 1000; \\ Max

\\ HE_trigger_frame.TrigCommonField.MoreTF = FALSE;

\\ HE_trigger_frame.TrigCommonField.CSRequired = FALSE;

\\ HE_trigger_frame.TrigCommonField.UlBw = TB_BW_20MHZ;

\\ HE_trigger_frame.TrigCommonField.LTFType = LTF_1_GI_1_6uS;

\\ HE_trigger_frame.TrigCommonField.LTFMode = MU_MIMO_SINGLE_STREAM;

\\ HE_trigger_frame.TrigCommonField.LTFSymbol = 0;

\\ HE_trigger_frame.TrigCommonField.UlSTBC = FALSE;

\\ HE_trigger_frame.TrigCommonField.LdpcESS = TRUE;

\\ HE_trigger_frame.TrigCommonField.ApTxPwr = 0

\\ HE_trigger_frame.TrigCommonField.PreFecPadFct = 1;

\\ HE_trigger_frame.TrigCommonField.PeDisambig = 0;

\\ HE_trigger_frame.TrigCommonField.SpatialReuse = 65535;

\\ HE_trigger_frame.TrigCommonField.Doppler = FALSE;

\\ HE_trigger_frame.TrigCommonField.HeSig2 = 0x1FF; \\ reserved


TrigCommonField=0;1000;0;0;0;1;0;0;0;1;0;1;0;65535;0;511


\\configure userinfo field of trigger frame

\\ HE_trigger_frame.TrigUserInfoField.AID12 = (5 & 0xFFF);

\\ HE_trigger_frame.TrigUserInfoField.RUAllocReg = 0;

\\ HE_trigger_frame.TrigUserInfoField.RUAlloc = 61; \\ 53 (106 tones)

\\ HE_trigger_frame.TrigUserInfoField.UlCodingType = CODING_TYPE_LDPC;

\\ HE_trigger_frame.TrigUserInfoField.UlMCS = 0;

\\ HE_trigger_frame.TrigUserInfoField.UlDCM = FALSE;

\\ HE_trigger_frame.TrigUserInfoField.SSAlloc = 0;

\\ HE_trigger_frame.TrigUserInfoField.UlTargetRSSI = 80;


TrigUserInfoField=5;0;61;1;0;0;0;80


\\configure trigger dependent user info field

\\ HE_trigger_frame.BasicTrigUserInfo.MPDU_MU_SF = MPDU_SPACING_MULT_1;

\\ HE_trigger_frame.BasicTrigUserInfo.TID_AL = 0;

\\ HE_trigger_frame.BasicTrigUserInfo.AC_PL = FALSE;

\\ HE_trigger_frame.BasicTrigUserInfo.Pref_AC = TB_AC_VO;

BasicTrigUserInfo=0;0;0;0

===================================================================

If there are any errors in this description, please let me know.

Also, if there are any other methods (ones that do not use a file), please let me know.

Re: IW611 RU setup

Hello @SA2 


Could you share test logs and captured spectrum?


Best Regards

Shaun

Re: IW611 RU setup

Hello, Shaun.
Thank you for your reply.
I’m sharing a screenshot of the spectrum.

captured spectrum.png


Re: IW611 RU setup

Hello @SA2 


Could you share cmd you issued on both golden unit and DUT? Including labtool return value


Best Regards

Shaun

Re: IW611 RU setup

Hello, Shaun.

There is something we would like to confirm before providing the command.

We have reviewed Chapter 12, but all RF tests must be performed using conducted measurements.
(The test is performed with the DUT sample for conducted measurements connected to the spectrum analyzer via an SMA cable.)

Therefore, if we are performing conducted measurements using only one set of DUTs, should we refer to Chapter 12.2 ?

Re: IW611 RU setup

Hello @SA2 


It is recommend to use standard test methods to measure. So that we could easy compare with our test report and find out if there are any issue.


Best Regards

Shaun

タグ(1)
評価なし
バージョン履歴
最終更新日:
2 週間前
更新者: