2397256_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2397256_en-US

2397256_en-US

"8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

i am using "8MPLUSLPD4-EVK"  . I am trying build the BSP but i am facing some build issue. Please help on this issue. Please let me know if you need more information.

error logs:

dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/project/imx-yocto-bsp/build$ bitbake core-image-minimal
ERROR: Attempting to set server environment: Unable to update the server configuration with local parameters: Traceback (most recent call last):
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/command.py", line 91, in runCommand
result = command_method(self, commandline)
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/command.py", line 291, in updateConfig
command.cooker.updateConfigOpts(options, environment, cmdline)
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 471, in updateConfigOpts
self.reset()
~~~~~~~~~~^^
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 1741, in reset
self.handlePRServ()
~~~~~~~~~~~~~~~~~^^
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 337, in handlePRServ
self.hashserv.serve_as_process(log_level=logging.WARNING)
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^^^^^^
File "/home/dasmiddepogu/NXP/project/imx-yocto-bsp/sources/poky/bitbake/lib/bb/asyncrpc/serv.py", line 402, in serve_as_process
self.process.start()
~~~~~~~~~~~~~~~~~~^^
File "/usr/lib/python3.14/multiprocessing/process.py", line 121, in start
self._popen = self._Popen(self)
~~~~~~~~~~~^^^^^^
File "/usr/lib/python3.14/multiprocessing/context.py", line 230, in _Popen
return _default_context.get_context().Process._Popen(process_obj)
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^
File "/usr/lib/python3.14/multiprocessing/context.py", line 306, in _Popen
return Popen(process_obj)
File "/usr/lib/python3.14/multiprocessing/popen_forkserver.py", line 35, in __init__
super().__init__(process_obj)
~~~~~~~~~~~~~~~~^^^^^^^^^^^^^
File "/usr/lib/python3.14/multiprocessing/popen_fork.py", line 20, in __init__
self._launch(process_obj)
~~~~~~~~~~~~^^^^^^^^^^^^^
File "/usr/lib/python3.14/multiprocessing/popen_forkserver.py", line 47, in _launch
reduction.dump(process_obj, buf)
~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^^^
File "/usr/lib/python3.14/multiprocessing/reduction.py", line 60, in dump
ForkingPickler(file, protocol).dump(obj)
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^^^^^
_pickle.PicklingError: Can't pickle local object .run at 0x7802f7325380>
when serializing dict item '_target'
when serializing multiprocessing.context.Process state
when serializing multiprocessing.context.Process object


repo details:

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap
-m imx-6.6.36-2.1.0.xml
$ repo sync

$ DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build


Linux host PC details:
PRETTY_NAME="Ubuntu 26.04 LTS"
NAME="Ubuntu"
VERSION_ID="26.04"
VERSION="26.04 (Resolute Raccoon)"
VERSION_CODENAME=resolute
ID=ubuntu
ID_LIKE=debian
HOME_URL="https://www.ubuntu.com/"
SUPPORT_URL="https://help.ubuntu.com/"
BUG_REPORT_URL="https://bugs.launchpad.net/ubuntu/"
PRIVACY_POLICY_URL="https://www.ubuntu.com/legal/terms-and-policies/privacy-policy"
UBUNTU_CODENAME=resolute
LOGO=ubuntu-logo



Host PC configuration:
Architecture: x86_64
CPU op-mode(s): 32-bit, 64-bit
Address sizes: 42 bits physical, 48 bits virtual
Byte Order: Little Endian
CPU(s): 16
On-line CPU(s) list: 0-15
Vendor ID: GenuineIntel
Model name: Intel(R) Core(TM) Ultra 7 255H
CPU family: 6
Model: 197
Thread(s) per core: 1
Core(s) per socket: 16
Socket(s): 1
Stepping: 2
CPU(s) scaling MHz: 17%
CPU max MHz: 5100.0000
CPU min MHz: 400.0000

DDR size : 32GB





i.MX8ULPRe: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello @middepogudas 

Hope you are doing very well.


The imx-linux-scarthgap BSP was validated on supported in Ubuntu 22.04 and Ubuntu 24.04.


Ubuntu 26.04 uses Python 3.14 by default and seems the Bitbake version in that BSP is not fully compatible with Python 3.14.


I recommend to you to compile using Ubuntu 24.04 LTS or Ubuntu 22.04 LTS until Ubuntu 26.04 LTS is fully supported.


Also, you can try using a virtual environment with python 3.12.



Best regards,

Salas.


Re: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

i flashed Ubuntu to 24.04 still i am facing build issue.. Please find build error logs. Please help on this build issue.


OS info: 

asmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/DOC$ cat /etc/os-release
PRETTY_NAME="Ubuntu 24.04.4 LTS"
NAME="Ubuntu"
VERSION_ID="24.04"
VERSION="24.04.4 LTS (Noble Numbat)"
VERSION_CODENAME=noble
ID=ubuntu
ID_LIKE=debian
HOME_URL="https://www.ubuntu.com/"
SUPPORT_URL="https://help.ubuntu.com/"
BUG_REPORT_URL="https://bugs.launchpad.net/ubuntu/"
PRIVACY_POLICY_URL="https://www.ubuntu.com/legal/terms-and-policies/privacy-policy"
UBUNTU_CODENAME=noble
LOGO=ubuntu-logo
dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/DOC$



build error logs:

You can now run 'bitbake '

Common targets are:
core-image-minimal
meta-toolchain
meta-toolchain-sdk
adt-installer
meta-ide-support

Your build environment has been configured with:

MACHINE=imx8mp-lpddr4-evk
SDKMACHINE=i686
DISTRO=fsl-imx-xwayland
EULA=
BSPDIR=
BUILD_DIR=.

dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/DOC$ DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build

dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/imx-yocto-bsp/build$ bitbake core-image-minimal
NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% | | ETA: --:--:--
Loaded 0 entries from dependency cache.
Parsing recipes: 100% |##################################################################################################################################################################################################################| Time: 0:00:55
Parsing of 3643 .bb files complete (0 cached, 3643 parsed). 5719 targets, 375 skipped, 17 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-24.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:f43f393ef0246b7bee6eed8bcf8271cf2b8cdf40"
meta-oe
meta-multimedia
meta-python = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-freescale = "HEAD:0f8091c63dd8805610c09b08409bc58492a3b16f"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:92ad51ef3cc7f132238f1ae6c8e81432f2a69cc7"
meta-nxp-demo-experience = "HEAD:8fd7154c05b716e9635279047f65785399432d88"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:783becb4b5716d989f50db95b7133d38eae5b47b"
meta-arm
meta-arm-toolchain = "HEAD:1b85bbb4cab9658da3cd926c62038b8559c5c64e"
meta-clang = "HEAD:fe561f41aef0cff9e6f96730ab59f28dca2eb682"
meta-gnome
meta-networking
meta-filesystems = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:6a80f140e387621f62964209a2e07d3bcfb125ce"

NOTE: Fetching uninative binary shim http://downloads.yoctoproject.org/releases/uninative/4.5/x86_64-nativesdk-libc-4.5.tar.xz;sha256sum=... (will check PREMIRRORS first)
Sstate summary: Wanted 2656 Local 0 Mirrors 0 Missed 2656 Current 0 (0% match, 0% complete)######################################################################################################################## | ETA: 0:00:00
Initialising tasks: 100% |###############################################################################################################################################################################################################| Time: 0:00:04
NOTE: Executing Tasks
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
File "/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/bitbake/bin/bitbake-worker", line 278, in child
bb.utils.disable_network(uid, gid)
File "/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py", line 1696, in disable_network
with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_unpack) failed with exit code '1'
ERROR: PermissionError: [Errno 1] Operation not permitted

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
File "/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/bitbake/bin/bitbake-worker", line 278, in child
bb.utils.disable_network(uid, gid)
File "/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/bitbake/lib/bb/utils.py", line 1696, in disable_network
with open("/proc/self/uid_map", "w") as f:
PermissionError: [Errno 1] Operation not permitted

ERROR: Task (/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_prepare_recipe_sysroot) failed with exit code '1'
NOTE: Tasks Summary: Attempted 34 tasks of which 0 didn't need to be rerun and 2 failed.

Summary: 2 tasks failed:
/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_unpack
/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-extended/texinfo-dummy-native/texinfo-dummy-native.bb:do_prepare_recipe_sysroot
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.
dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/imx-yocto-bsp/build$


Thank you,,

Das Middepogu

Re: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

Can you please help below BSP build error?



dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/lp_imx-yocto-bsp/build$ python3 --version
Python 3.12.3

dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/lp_imx-yocto-bsp/build$ cat /etc/os-release
PRETTY_NAME="Ubuntu 24.04.4 LTS"
NAME="Ubuntu"
VERSION_ID="24.04"
VERSION="24.04.4 LTS (Noble Numbat)"
VERSION_CODENAME=noble
ID=ubuntu
ID_LIKE=debian
HOME_URL="https://www.ubuntu.com/"
SUPPORT_URL="https://help.ubuntu.com/"
BUG_REPORT_URL="https://bugs.launchpad.net/ubuntu/"
PRIVACY_POLICY_URL="https://www.ubuntu.com/legal/terms-and-policies/privacy-policy"
UBUNTU_CODENAME=noble
LOGO=ubuntu-logo
dasmiddepogu@dasmidde



| ERROR: configure failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1539 tasks of which 1519 didn't need to be rerun and 2 failed.

Summary: 2 tasks failed:
/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_package
/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure
Summary: There were 2 WARNING messages.
Summary: There were 3 ERROR messages, returning a non-zero exit code.
dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/lp_imx-yocto-bsp/build$ bitbake core-image-minimal

Re: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

please find the python version which i am using. Please find below build errror logs and help us how to fix for success-full build. please find config.log file as attached


asmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/lp_imx-yocto-bsp/build$ python3 --version
Python 3.12.3
dasmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~


asmiddepogu@dasmiddepogu-ThinkPad-P14s-Gen-6:~/NXP/lp_imx-yocto-bsp/build$ bitbake core-image-minimal
WARNING: Host distribution "ubuntu-24.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |####################################################################################################################################################################################################################| Time: 0:00:00
Loaded 5303 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.4.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-24.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.1-mickledore"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:0a98281d37b0bd8dc1548c390216cb3978e36e0e"
meta-oe
meta-multimedia
meta-python = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842"
meta-freescale = "HEAD:9b00d40b787c2b7105ce209f5635cc1a0cab81ca"
meta-freescale-3rdparty = "HEAD:93ba05e3a16a028b770fa1e813b13eb87a59ac63"
meta-freescale-distro = "HEAD:b09c18a3f649f0cf1b40432bb39e76ba16fe94e2"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:6efe87f014c5bdcbda30f06156ee11d8bc3dc7fe"
meta-nxp-demo-experience = "HEAD:7f34a32c7877e55e87b6a99e90da4128ed632bf2"
meta-arm
meta-arm-toolchain = "HEAD:0e043288fd0b17fbf31cf00ae33045107a991144"
meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang = "HEAD:af4dcba009ba98250315520f3003fde4ee164cce"
meta-gnome
meta-networking
meta-filesystems = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842"
meta-qt6 = "HEAD:1406d0a85525a71fe5d7892d7f915404290a78ad"
meta-parsec
meta-tpm = "HEAD:d7db0a3bd1a8639df7570483f003ce00cbe274a2"
meta-virtualization = "HEAD:56593e277a377157944a6676e57497066b770a35"

WARNING: Your host glibc version (2.39) is newer than that in uninative (2.37). Disabling uninative so that sstate is not corrupted.
Initialising tasks: 100% |###############################################################################################################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 833 Local 2 Mirrors 0 Missed 831 Current 940 (0% match, 53% complete)
NOTE: Executing Tasks
ERROR: linux-libc-headers-6.1-r0 do_package: Error executing a python function in exec_func_python() autogenerated:

The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_func_python() autogenerated', lineno: 2, function:
0001:
*** 0002:perform_packagecopy(d)
0003:
File: '/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/classes-global/package.bbclass', lineno: 355, function: perform_packagecopy
0351: rpath_replace (dvar, d)
0352:}
0353:perform_packagecopy[cleandirs] = "${PKGD}"
0354:perform_packagecopy[dirs] = "${PKGD}"
*** 0355:
0356:python populate_packages () {
0357: oe.package.populate_packages(d)
0358:}
0359:populate_packages[dirs] = "${D}"
File: '/usr/lib/python3.12/subprocess.py', lineno: 466, function: check_output
0462: else:
0463: empty = b''
0464: kwargs['input'] = empty
0465:
*** 0466: return run(*popenargs, stdout=PIPE, timeout=timeout, check=True,
0467: **kwargs).stdout
0468:
0469:
0470:class CompletedProcess(object):
File: '/usr/lib/python3.12/subprocess.py', lineno: 571, function: run
0567: # We don't call process.wait() as .__exit__ does that for us.
0568: raise
0569: retcode = process.poll()
0570: if check and retcode:
*** 0571: raise CalledProcessError(retcode, process.args,
0572: output=stdout, stderr=stderr)
0573: return CompletedProcess(process.args, retcode, stdout, stderr)
0574:
0575:
Exception: subprocess.CalledProcessError: Command 'tar --exclude=./sysroot-only -cf - -C /home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/linux-libc-headers/6.1-r0/image -p -S . | tar -xf - -C


/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/linux-libc-headers/6.1-r0/package' returned non-zero exit status 2.

Subprocess output:
got *at() syscall for unknown di



ar: ./usr/include/asm-generic/poll.h: Cannot open: No such file or directory
tar: Exiting with failure status due to previous errors

ERROR: Logfile of failure stored in: /home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/linux-libc-headers/6.1-r0/temp/log.do_package.75498
ERROR: Task (/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_package) failed with exit code '1'
ERROR: libxcrypt-4.4.33-r0 do_configure: configure failed
ERROR: libxcrypt-4.4.33-r0 do_configure: ExecutionError('/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/libxcrypt/4.4.33-r0/temp/run.do_configure.75465', 1, None, None)
ERROR: Logfile of failure stored in: /home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/libxcrypt/4.4.33-r0/temp/log.do_configure.75465
Log data follows:


NOTE: The following config.log files may provide further information.
| NOTE: /home/dasmiddepogu/NXP/lp_imx-yocto-bsp/build/tmp/work/armv8a-poky-linux/libxcrypt/4.4.33-r0/build/config.log
| ERROR: configure failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1546 tasks of which 1537 didn't need to be rerun and 2 failed.

Summary: 2 tasks failed:
/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_6.1.bb:do_package
/home/dasmiddepogu/NXP/lp_imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure
Summary: There were 2 WARNING messages.
Summary: There were 3 ERROR messages, returning a non-zero exit code.


Thank you

Re: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

Any suggestions on my above build error?


Das Middepogu

Re: "8MPLUSLPD4-EVK" build issue with Ubuntu 26.04 LTS

Hello NXP,

Please help to give some input how to fix the below build error?


I am using ubuntu 24.04 and python version 3.8. 

build command : imx-yocto-bsp/build$ bitbake core-image-minimal


build error:

WARNING: exit code 1 from a shell command.
ERROR: Task (/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2891 tasks of which 16 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/dasmiddepogu/NXP/imx-yocto-bsp/sources/poky/meta/recipes-core/libxcrypt/libxcrypt_4.4.33.bb:do_configure
Summary: There were 78 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.



Tags (1)
No ratings
Version history
Last update:
2 weeks ago
Updated by: