2396034_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2396034_en-US

2396034_en-US

MPC5746C FXOSC output frequency

Part: MPC5746C (Power Architecture Z4, SDK: NXP MPC57xx platform SDK).
In the manual of MPC5746C, it is stated that FXOSC provides 8 -40 MHz output frequency. Please help me in finding the output frequency provided by FXOSC for the following configurations?
1. FXOSC_CTL: OSCBYP = 0 and OSCM = LCP

2. FXOSC_CTL: OSCBYP = 0 and OSCM = FSP

3. FXOSC_CTL: OSCBYP = 1 and OSCM = LCP

4. FXOSC_CTL: OSCBYP = 1 and OSCM = FSP

Please consider default values for the other register fields. Thanks.

Re: MPC5746C FXOSC output frequency

Thanks for your response @petervlna

How can we find the frequency provided by the crystal/resonator(OSCBYP = 0) and external clock(OSCBYP = 1)?

Re: MPC5746C FXOSC output frequency

Hello,

The FXOSC module does not generate a specific frequency based on the OSCBYP and OSCM settings. The FXOSC output frequency is always equal to the frequency of the external source connected to FXOSC (crystal/resonator when OSCBYP=0, or external clock when OSCBYP=1), within the supported range of 8–40 MHz.


Therefore, for all four configurations listed, the FXOSC output frequency is simply the external input frequency. The OSCM setting (LCP/FSP) affects the oscillator operating mode, but does not change the clock frequency.

Best regards,

Peter

Re: MPC5746C FXOSC output frequency

@petervlna please provide your support for my FXOSC query mentioned above. 

Re: MPC5746C FXOSC output frequency

How can we find the frequency provided by the crystal/resonator(OSCBYP = 0) and external clock(OSCBYP = 1)?

Please let me know on the above question @petervlna. I want to use FXOSC as clock source for a timer. Based on the frequency it provides i can load a count value into the timer register

Re: MPC5746C FXOSC output frequency

Hello,

The MPC5746C does not provide a way to measure or determine the FXOSC frequency from the FXOSC registers. The frequency must be known from the hardware design:

  • OSCBYP = 0: FXOSC frequency equals the frequency of the external crystal/resonator fitted on the board.
  • OSCBYP = 1: FXOSC frequency equals the frequency of the external clock signal applied to the FXOSC input pin.

To use FXOSC as a timer clock source, the application must use the frequency specified in the board schematic or clock design (for example, 8 MHz, 16 MHz, 40 MHz, etc.) when calculating the timer count value. The OSCBYP and OSCM settings do not affect the frequency itself.

Best regards,

Peter

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-24-2026 04:33 AM
更新者: