2394920_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394920_en-US

2394920_en-US

How to Configure BLE MAC Address on a Custom RW610 Board

Hi NXP Team,

I have a custom RW610 board on which I am testing one of the BLE SDK example projects.

When the board starts advertising, the BLE MAC address is displayed as 88:88:88:88:88:88. However, when I tested the same SDK example on the FRDM-RW612 EVK, it advertised with a unique Bluetooth MAC address.

I would like to understand:

  • How is the BLE MAC address assigned on the RW610?
  • How can I configure or program a unique BLE MAC address for my custom RW610 board?
  • Is the MAC address expected to be stored in external flash or generated by software?
  • Are there any SDK APIs or board configuration changes required to set the BLE MAC address?

Any guidance or references would be greatly appreciated.

Thanks & Regards,
Prathyush.

Re: How to Configure BLE MAC Address on a Custom RW610 Board

Hi,

The FRDM-RW612 already comes with a programmed BD address.

For your custom board, you will need to program a BD address into the OTP memory.

Please refer to the Calibration Structure for RW61x application note: https://www.nxp.com/docs/en/application-note/AN13639.pdf

For testing purposes, you can use a static BD address. For example, you can create and select one using the id-create command from the Bluetooth shell. Please refer to UM11799 for additional details.

Regards,
Daniel.

Re: How to Configure BLE MAC Address on a Custom RW610 Board

Hi Daniel,

Thank you so much for your guidance and support.

I implemented a temporary static BLE address for testing on my custom RW610 board.

I really appreciate your help.

Regards,
Prathyush

Tags (1)
No ratings
Version history
Last update:
‎07-17-2026 02:36 AM
Updated by: