2394854_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2394854_en-US

2394854_en-US

PNEV5180B 2.0 PN5180 Altium Schematics

Are the PNEV5180B 2.0 PN5180 schematics available in ALtium format ?

ALso PCB would be useful , mainly for the NFC antenna.


We want to use the PN5180 and want to get  up and working asap

Re: PNEV5180B 2.0 PN5180 Altium Schematics

Hello @David-Lightbug

Hope you are doing well.

Please accept my apologies, PN5180 design files are not available. Perhaps you could refer to the PN5180 Evaluation board quick start guide, which includes some pictures showing the relevant schematics. Also, please refer to the PN5180 Antenna design.

If possible, I will recommend considering PN5190 | NFC Frontend for payment. Following design files related to PNEV5190BP are available:

Module board
Base board

Regards,
Eduardo.

Re: PNEV5180B 2.0 PN5180 Altium Schematics

Hi,



Going through the altium schematics , they all appear to be the BGA package/  You have the PNEV5190M  (BGA packagein cct diagram) and   PNEV5190BP also BGA.

I have found the evaluation board manual, PNEV5180B that shows the QFN package but not the altium files.


Can you help.

Re: PNEV5180B 2.0 PN5180 Altium Schematics

Hi,

We offer a NFC Reader Library for PN5190. This library is designed for some Host MCUs from NXP's portfolio, such as LPC1769 and Kinetis K82; porting the functionality to a third-party platform is out of our support and must be done entirely by the customers. You can refer to the following articles and use them as a reference for the porting:

- Using NFC Reader Library with LPC55S69

- NFC Reader Library Porting FRDM_K64F

- NFC Reader Library Porting to i.MX RT1050 - NXP Community

The available design files for PN5190 are based on our Development Board (PNEV5190BP), which embeds the BGA package. There is also a reference design for the VFLGA40 package: Module board PN5190 HVQFN design files; however, the purpose of this file is to illustrate the required connections for this specific package.

Regards,
Eduardo.

Re: PNEV5180B 2.0 PN5180 Altium Schematics

Hi,


Thanks for your quick reply.

I will change to use the PN5190.

Are the code compatible/ similar to the PN5180 , the reason I am asking is that I have noticed there are Arduino libraries  for the PN5180 but not the PN5180.


DO you have libraires - we just want to get up and going quickly with the product.  The board design is likely to be ready and made in less than two weeks.

Thanks

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-16-2026 03:29 AM
更新者: