2394735_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394735_en-US

2394735_en-US

SOM module recommendation to replace AM3354
Hi Expert,
 
Any recommendation for SOM module to replace TI AM3354 with following feature needed with Module TP: US$40~U$44
 
Featured Needed:
Ethernet
SGMII/RGMII
SPI
24-bits LCD controller
eMMC 8GB
RAM 512MB 
 
Please recommend it can meet close to target price. 
 
Best rgds, KPK
 
 
Re: SOM module recommendation to replace AM3354

Both TechNexion and Variscite support APAC customers. For Singapore, TechNexion may provide more convenient regional support due to its Taiwan headquarters. I recommend contacting TechNexion ([email protected]) and Variscite ([email protected]) directly to discuss Singapore distribution coverage, local support resources, stocking policy, and design-win support

Re: SOM module recommendation to replace AM3354

hi Yiping, i also just study the Variscite DART-6UL or TechNexian PICO-IMX6ULL.

Not sure if they have any local support in APAC region?  Do you have any contact point to share?



Re: SOM module recommendation to replace AM3354

1. NXP i.MX93 SOM (Best Long-Term Option)

The i.MX93 supports:

  • 24-bit Parallel RGB Display
  • eMMC 5.1 
  • Multiple SPI interfaces 
  • Gigabit Ethernet with TSN

Pros

  • Current generation MPU
  • Long NXP longevity roadmap
  • Lower power than AM335x
  • Linux support active for many years

Cons

  • Native SGMII not directly available like Layerscape/i.MX95
  • SOM price typically exceeds US$45 once 512MB DDR + 8GB eMMC are included

Expected SOM Price

  • Approximately US$45–60 depending on volume

2. NXP i.MX6ULL SOM (Best Price Match)

The i.MX6ULL provides:

  • 24-bit Parallel RGB LCD interface up to WXGA
  • eMMC support
  • SPI ports
  • 512MB DDR variants readily available

Typical SOM configurations already exist with:

  • 512MB DDR3
  • 8GB eMMC
  • Dual Ethernet

Pros

  • Closest price to AM3354
  • Mature Linux BSP
  • Large SOM ecosystem
  • Easy migration from AM335x-style designs

Cons

  • No native SGMII
  • Ethernet limited to Fast Ethernet (10/100) on most modules

Expected SOM Price

  • US$25–40 in production volumes
  •  

For native SGMII, you'll generally move to:

  • i.MX94x / i.MX95 families 
  • Layerscape LS1028A/LS1043A

These usually push SOM pricing well beyond US$44.

Tags (1)
No ratings
Version history
Last update:
‎07-15-2026 02:30 AM
Updated by: