2394655_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394655_en-US

2394655_en-US

How to configure the PF53 to output 0.8V?

Hello,

I am using S32G399, MVR5510AMDALES, and MPF5302AMDA0ES for my design.

According to the datasheet, the MPF5302AMDA0ES is a non-programmed device. How can I configure the MPF5302AMDA0ES to output 0.8V to the S32G399 Core? Supply uses it.

I originally wanted to program the S32G399 via JTAG so that the S32G399 could configure the MPF5302AMDA0ES to output 0.8V via IIC. However, there is no 0.8V being supplied to the S32G399 core. Supply cannot connect via JTAG. This seems to be a vicious cycle.

MichaelTao_0-1784009570077.pngMichaelTao_0-1784009570077.png


Re: PF53如何配置输出0.8VOkay, thank you. I'll post it again on the new page.Re: PF53如何配置输出0.8V

Hello, @MichaelTao

Hello, generally speaking

1. During the engineering development phase, customers are allowed to use the NXP GUI and socketed evaluation board to perform OTP emulation/programming (which can then be used with the S32G).
2. For custom OTPs used in the mass production stage, you need to contact NXP's sales channel/distributor; mass production OTP programming should be completed by NXP or a recommended third party.

Since this forum primarily addresses issues related to the S32G itself, if you require further details for confirmation, please post in the following forums where dedicated product support engineers will provide further assistance. Thank you for your understanding.


BR

Chenyin


BR

Chenyin

Tags (1)
No ratings
Version history
Last update:
‎07-15-2026 03:28 AM
Updated by: