2394184_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394184_en-US

2394184_en-US

AP1302 MIPI CSI Streaming Issue on FRDM i.MX93

Hello,

I am using an FRDM i.MX93 board with the X-RPI-CAM-MIPI A1 camera module.

The issue I am facing is that I am unable to capture the MIPI CSI stream from this setup.

I have placed the firmware binary ap1302_60fps_ar0144_27M_2Lane_awb_tuning.bin in the following location: "/lib/firmware"

During boot, I see that the AP1302 is detected successfully, but when I attempt to start video streaming, VIDIOC_STREAMON fails with a "Broken pipe" error.

Below are the relevant logs.

Kernel log:

root@imx93evk:~# dmesg | grep ap1302
[    0.340980] /soc@0/bus@42000000/i2c@42530000/ap1302_mipi@3c: Fixed dependency cycle(s) with /soc@0/bus@42800000/csi@4ae00000
[    0.371014] /soc@0/bus@42800000/csi@4ae00000: Fixed dependency cycle(s) with /soc@0/bus@42000000/i2c@42530000/ap1302_mipi@3c
...
[   10.088832] ap1302 2-003c: AP1302 revision 0.2.6 detected

Streaming test:

root@imx93evk:~# v4l2-ctl -d /dev/video0 \
    --verbose \
    --stream-mmap=3 \
    --stream-count=10

VIDIOC_QUERYCAP: ok
VIDIOC_REQBUFS returned 0 (Success)
VIDIOC_CREATE_BUFS returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_G_FMT returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_STREAMON returned -1 (Broken pipe)

Could you please help me understand why VIDIOC_STREAMON is failing with a "Broken pipe" error?

Is there any additional configuration required for the AP1302 firmware, device tree, media pipeline, or sensor initialization before streaming can start successfully?

Furthermore, i am using "LF_v6.18.2-1.0.0_images_IMX93EVK" pre-built images for now.

Please let me know if you need any additional logs or information.

Thank you for your support.

Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93

Discussing with the AE team.

Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93

Hello @yipingwang 

Thank you for your response.

Please find my answers below for your reference.

1. Firmware Location

I tried both the recommended firmware locations as well as each location individually. The camera probe is successful only when using ap1302_ar0144_single_fw.bin.

root@imx93evk:~# ls -la /lib/firmware/ap1302_ar0144_single_fw.bin
-rw-r--r-- 1 root root 80528 Aug  5 15:36 /lib/firmware/ap1302_ar0144_single_fw.bin

root@imx93evk:~# ls -la /lib/firmware/imx/camera/ap1302.fw
-rw-r--r-- 1 root root 80528 Aug  5 15:38 /lib/firmware/imx/camera/ap1302.fw

The AP1302 is detected successfully during boot.

root@imx93evk:~# dmesg | grep -i ap1302
...
[    9.962705] ap1302 2-003c: AP1302 revision 0.2.6 detected

However, I do not see any firmware loading messages related to AP1302 in the kernel log.


2. Software Environment

I am using the pre-built images provided for the FRDM i.MX93 board.

root@imx93evk:~# cat /proc/device-tree/model
NXP FRDM-IMX93

root@imx93evk:~# cat /proc/cmdline
console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw

The AP1302 is detected successfully, and the CSI/ISI devices are also present. I have attached the complete logs for your reference.


3. Media Pipeline

The media pipeline appears to be created correctly.

root@imx93evk:~# ls /dev/media0
/dev/media0

root@imx93evk:~# ls /dev/video*
/dev/video0  /dev/video1

The outputs from media-ctl show that the AP1302, CSI, and ISI entities are enabled. The complete media-ctl output is attached for your reference.


4. Additional Information

Please refer to the attached file fourth_point.txt for the requested information.


5. Streaming Failure

I do not see any additional kernel messages when the streaming command fails.

root@imx93evk:~# dmesg -c

root@imx93evk:~# v4l2-ctl -d /dev/video0 --stream-mmap=3 --stream-count=10
VIDIOC_STREAMON returned -1 (Broken pipe)

root@imx93evk:~# dmesg

The dmesg output remains empty after the failure, so there are no additional kernel logs to help identify the root cause.

Since the AP1302 is detected successfully, the media graph is created correctly, and no kernel errors are reported during VIDIOC_STREAMON, could you please suggest what additional checks or debugging steps I should perform to identify why streaming fails with a "Broken pipe" error?

Thank you for your support.


root@imx93evk:~# v4l2-ctl --list-devices
mxc-isi-cap (platform:4ae40000.isi):
        /dev/video0
        /dev/video1
        /dev/media0

root@imx93evk:~# v4l2-ctl -d /dev/video0 --all
Driver Info:
        Driver name      : mxc-isi
        Card type        : mxc-isi-cap
        Bus info         : platform:4ae40000.isi
        Driver version   : 6.18.2
        Capabilities     : 0xa4201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
                Device Capabilities
        Device Caps      : 0x24201000
                Video Capture Multiplanar
                I/O MC
                Streaming
                Extended Pix Format
Media Driver Info:
        Driver name      : mxc-isi
        Model            : FSL Capture Media Device
        Serial           : 
        Bus info         : platform:4ae40000.isi
        Media version    : 6.18.2
        Hardware revision: 0x00000000 (0)
        Driver version   : 6.18.2
Interface Info:
        ID               : 0x0300000a
        Type             : V4L Video
Entity Info:
        ID               : 0x00000008 (8)
        Name             : mxc_isi.0.capture
        Function         : V4L2 I/O
        Pad 0x01000009   : 0: Sink
          Link 0x0200000c: from remote pad 0x1000007 of entity 'mxc_isi.0' (Video Pixel Formatter): Data, Enabled, Immutable
Priority: 2
Video input : 0 (mxc_isi.0.capture: ok)
Format Video Capture Multiplanar:
        Width/Height      : 1920/1080
        Pixel Format      : 'YUYV' (YUYV 4:2:2)
        Field             : None
        Number of planes  : 1
        Flags             : 
        Colorspace        : sRGB
        Transfer Function : sRGB
        YCbCr/HSV Encoding: ITU-R 601
        Quantization      : Limited Range
        Plane 0           :
           Bytes per Line : 3840
           Size Image     : 4147200

User Controls

                horizontal_flip 0x00980914 (bool)   : default=0 value=0 flags=0x00001000
                  vertical_flip 0x00980915 (bool)   : default=0 value=0 flags=0x00001000
                alpha_component 0x00980929 (int)    : min=0 max=255 step=1 default=0 value=0 flags=0x00001000
root@imx93evk:~# media-ctl -p
Media controller API version 6.18.2

Media device information
------------------------
driver          mxc-isi
model           FSL Capture Media Device
serial          
bus info        platform:4ae40000.isi
hw revision     0x0
driver version  6.18.2

Device topology
- entity 1: crossbar (3 pads, 3 links, 1 route)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev0
        routes:
                0/0 -> 2/0 [ACTIVE]
        pad0: SINK,MUST_CONNECT
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                <- "csidev-4ae00000.csi":1 [ENABLED,IMMUTABLE]
        pad1: SINK,MUST_CONNECT
                <- "mxc_isi.output":0 [ENABLED,IMMUTABLE]
        pad2: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                -> "mxc_isi.0":0 [ENABLED,IMMUTABLE]

- entity 5: mxc_isi.0 (2 pads, 2 links, 0 routes)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev1
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 compose.bounds:(0,0)/1920x1080
                 compose:(0,0)/1920x1080]
                <- "crossbar":2 [ENABLED,IMMUTABLE]
        pad1: SOURCE
                [stream:0 fmt:YUV8_1X24/1920x1080 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
                 crop.bounds:(0,0)/1920x1080
                 crop:(0,0)/1920x1080]
                -> "mxc_isi.0.capture":0 [ENABLED,IMMUTABLE]

- entity 8: mxc_isi.0.capture (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/video0
        pad0: SINK
                <- "mxc_isi.0":1 [ENABLED,IMMUTABLE]

- entity 16: mxc_isi.output (1 pad, 1 link)
             type Node subtype V4L flags 0
        pad0: SOURCE
                -> "crossbar":1 [ENABLED,IMMUTABLE]

- entity 23: csidev-4ae00000.csi (2 pads, 2 links, 1 route)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev2
        routes:
                0/0 -> 1/0 [ACTIVE]
        pad0: SINK
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                <- "ap1302 2-003c":2 [ENABLED]
        pad1: SOURCE
                [stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                -> "crossbar":0 [ENABLED,IMMUTABLE]

- entity 28: ap1302 2-003c (3 pads, 2 links, 0 routes)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev4
        pad0: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                <- "ar0144 0":0 [ENABLED,IMMUTABLE]
        pad1: SINK
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
        pad2: SOURCE
                [stream:0 fmt:UYYVYY8_0_5X24/4224x4092 field:none colorspace:srgb
                 crop.bounds:(0,0)/1280x800
                 crop:(0,0)/1280x800]
                -> "csidev-4ae00000.csi":0 [ENABLED]

- entity 32: ar0144 0 (1 pad, 1 link, 0 routes)
             type V4L2 subdev subtype Sensor flags 0
             device node name /dev/v4l-subdev3
        pad0: SOURCE
                [stream:0 fmt:SGRBG12_1X12/1280x800 field:none colorspace:srgb]
                -> "ap1302 2-003c":0 [ENABLED,IMMUTABLE]

Best regards,
Milav

Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93

the AP1302 probe succeeding does not guarantee that the complete camera pipeline is configured and streaming. On i.MX93, a VIDIOC_STREAMON returned -1 (Broken pipe) typically means that one of the media pipeline components (AP1302 → MIPI CSI-2 receiver → ISI capture path) failed to start or negotiate a valid stream. Your log only confirms that the AP1302 I²C device was detected:

ap1302 2-003c: AP1302 revision 0.2.6 detected

but it does not confirm that:

  • the firmware was loaded successfully,
  • the correct DTB was used,
  • the media graph was created,
  • the CSI receiver is locked to incoming MIPI data,
  • the AP1302 has been configured with a matching output format.

First thing I would check: firmware location/name

For the FRDM-i.MX93 AP1302 support, NXP documentation indicates:

  1. Download ap1302_60fps_ar0144_27M_2Lane_awb_tuning.bin
  2. Rename it to ap1302.fw
  3. Place it in:

/lib/firmware/imx/camera/ap1302.fw

not simply /lib/firmware.

Please verify:

ls -l /lib/firmware/imx/camera/ap1302.fw


and check boot log:

dmesg | grep -i firmware

dmesg | grep -i ap1302

Look for messages such as:

request firmware

firmware loaded

failed to load firmware

Second check: are you using the correct DTB?

The release notes indicate AP1302 support is associated with the i.MX93 EVK device tree support.

Check:

cat /proc/device-tree/model

cat /proc/cmdline

and determine the actual DTB being loaded.

Also check:

dmesg | grep -i ap1302

dmesg | grep -i csi

dmesg | grep -i isi

Third check: verify media topology

Before trying v4l2-ctl, verify that the media graph exists:

Shell

media-ctl -p

Show more lines

You should see entities similar to:

ap1302

csi

isi

videoX

If /dev/media0 does not exist, the camera pipeline is not being created correctly. A very similar FRDM-i.MX93 AP1302 case showed:

media-ctl -p

Failed to enumerate /dev/media0

which indicated the media pipeline was not instantiated.

Please check:

ls -l /dev/media*


Fourth check: inspect the negotiated formats

Run:

v4l2-ctl --list-devices

and

v4l2-ctl -d /dev/video0 --all

also:

media-ctl -p

The AP1302 firmware normally outputs processed YUV formats rather than RAW Bayer. Another common failure is:

AP1302 outputs format A

ISI configured for format B

causing stream startup failure. A format mismatch often surfaces as STREAMON failure or CSI pipeline errors.

Fifth check: inspect CSI errors during STREAMON

Open another terminal and monitor:

dmesg -w

then run:

v4l2-ctl -d /dev/video0 \

--stream-mmap=3 \

--stream-count=10


Look for messages such as:

CSI timeout

frame start timeout

no data received

FIFO overflow

MIPI error

link not enabled


These messages usually reveal the real reason behind the Broken pipe.

Re: AP1302 MIPI CSI Streaming Issue on FRDM i.MX93

It's required to set up the pipeline using the following commands before capturing.

$ media-ctl -l "'ap1302 2-003c':2 -> 'csidev-4ae00000.csi':0 [1]"
$ media-ctl -V "'ap1302 2-003c':0 [fmt: UYVY8_1X16/1280x800 field:none]"
$ media-ctl -V "'ap1302 2-003c':2 [fmt: UYVY8_1X16/1280x800 field:none]"
$ media-ctl -V "'ar0144 0':0 [fmt: UYVY8_1X16/1280x800 field:none]"
$ media-ctl -V "'csidev-4ae00000.csi':1 [fmt: UYVY8_1X16/1280x800 field:none]"
$ media-ctl -V "'crossbar':2 [fmt: UYVY8_1X16/1280x800 field:none]"

Tags (1)
No ratings
Version history
Last update:
‎07-17-2026 02:35 AM
Updated by: