2393956_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2393956_en-US

2393956_en-US

Inquiry Regarding JTAG Debugger Support for LX2082A

Dear NXP Support Team,

I am developing a custom board based on the NXP LX2082A processor and am currently planning the hardware bring-up and debugging setup.

I would like to clarify whether SEGGER J-Link is officially supported for the following tasks on the LX2082A:

  • Initial board bring-up
  • JTAG debugging
  • Bare-metal debugging
  • TF-A and U-Boot debugging
  • Linux kernel debugging
  • Flash programming (if supported)

My development environment is Linux, and I plan to develop and build all software on a Linux host.

Could you please advise:

  1. Is SEGGER J-Link officially supported for the LX2082A?
  2. If yes, which J-Link models are supported?
  3. Are there any limitations compared to NXP-recommended debug solutions?
  4. If J-Link is not recommended, could you please suggest the officially supported hardware debugger(s) for the LX2082A?

I would appreciate any documentation or application notes related to JTAG debugging and board bring-up for the LX2082A.

Thank you for your assistance. I look forward to your guidance.

Kind regards.

Re: Inquiry Regarding JTAG Debugger Support for LX2082A

The NXP officially supported debugger is CWTAP.

You can use codewarrior Developer Suite Level for your application.

You can also download  Evaluation Edition(free-trial) from below link but it has 30-day time restriction

Every customer account (email address) can download the Evaluation Edition from the link below.

Please select “DOWNLOAD EVAL”.

https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools...

Please find the useful docuemnttation below:

 

ARMv8_Targeting_Manual.pdf

 

CodeWarrior TAP Probe User Guide

 

Layerscape Linux SDK User Guide

Clarification on CodeWarrior License After 30-Day Evaluation (CW TAP / QCVS / QCS)

Hello NXP Support,

I have a question regarding the 30-day CodeWarrior Evaluation Edition.

After the evaluation period expires:

  1. Will JTAG connection (using CW TAP) still work, or does CodeWarrior stop functioning completely?
  2. Will RCW generation/programming and flash programming still be available without a paid license?
  3. Can QCVS (QorIQ Configuration and Validation Suite) continue to be used after the trial expires, or does it also require a valid CodeWarrior license?
  4. For customers using only Linux command-line tools (U-Boot, Yocto, OpenOCD, etc.), is purchasing CodeWarrior recommended only for JTAG debugging, or is it mandatory for board bring-up?

I would appreciate your clarification on which features remain available after the evaluation period.

Thank you.

Re: Inquiry Regarding JTAG Debugger Support for LX2082A

1.  CodeWarrior function will stop.

2. No.

3. No. Need a valid license.

4. Linux debug could work without JTAG debugging, but DDR validation on each board, and first time flash should use the JTAG debugger(CW TAP) with CodeWarrior IDE.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-18-2026 02:28 AM
更新者: