We are planning to use this eMMC PTE4ABTE-32GX from PHISON with the IMX8M Processor. Please confirm whether this will support booting. Attaching the datasheet for reference.
Yes, based on the datasheet, the PHISON PTE4ABTE-32GX should support booting on the i.MX8M family (i.MX8MQ / i.MX8MM / i.MX8MN / i.MX8MP), provided it is connected to a USDHC interface according to the i.MX8M Hardware Design Guide.
Yes, the i.MX8ML (MIMX8ML5CVNKZAB) supports booting from an eMMC device connected through the USDHC interface. The PHISON PTE4ABTE-32GX is an eMMC 5.1 device and is expected to be compatible with the i.MX8ML boot flow when connected and configured according to the i.MX8M Hardware Design Guide.
@yipingwang Thanks for your response.
We are using MIMX8ML5CVNKZAB, which is an i.MX8ML device. In your response, only the i.MX8M family (i.MX8MQ / i.MX8MM / i.MX8MN / i.MX8MP) has been mentioned.
Could you please confirm whether the PHISON PTE4ABTE-32GX is also supported for booting with the i.MX8ML device when connected to the USDHC interface as per the hardware design guidelines?