2393376_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2393376_en-US

2393376_en-US

An error occurred while building the target device using GuiGuiDer2.0.0.

I have now created a guiguider project based on frdm_mcx947, using version 2.0.0, and selected ARM. The GCC version is 14.4.1.

I have already configured the arm gcc tool.

The following error message occurred during compilation: C:\Users\liujianhua>where arm-none-eabi-gcc
D:\tools\GCC14\14.2\bin\arm-none-eabi-gcc.exe

11:41:00INFObuild-target Started11:41:00INFOTarget Executor initialized11:41:00INFOBuilding target with armgcc toolchain...11:41:00INFOStarting ARM GCC build...11:41:00INFOSearching for ARM GCC toolchain in system PATH...11:41:00INFOExecuting: where arm-none-eabi-gcc11:41:00INFO'where' �����ڲ����ⲿ���Ҳ���ǿ����еij���
���������ļ���11:41:00ERRORARM GCC not found in system PATH: Command failed with code 1: 'where' �����ڲ����ⲿ���Ҳ���ǿ����еij���
�����������
11:41:00ERRORARM GCC build error: ARM GCC toolchain not found. Please install it and add to system PATH.11:41:00ERRORBuild failed: ARM GCC toolchain not found. Please install it and add to system PATH.11:41:00ERROROperation failed: ARM GCC toolchain not found. Please install it and add to system PATH.

I was successful in finding the compiler tools using cmd:

C:\Users\liujianhua>where arm-none-eabi-gcc
D:\tools\GCC14\14.2\bin\arm-none-eabi-gcc.exe
Tags (1)
No ratings
Version history
Last update:
‎07-11-2026 02:29 AM
Updated by: