This guide provides step-by-step instructions on how to verify successful communication and the runtime software environment to interface with the Ara240 module with the FRDM i.MX 95 Pro development board.
Ara240 Module [Back view]Ara240 Module [Back view]
Ara240 Module [Top view]Ara240 Module [Top view]
This section explains how to connect Ara240, a discrete module, to the FRDM i.MX 95 Pro development board. The instructions in the FRDM i.MX 95 Pro Getting Start Guide will walk you through the boot-up process for the pre-loaded Embedded Linux image on the board and how to connect the USB debug cable. For additional details, see the official FRDM i.MX 95 Pro Development Board documentation.
References:
FRDM i.MX 95 Pro Quick Start Guide
FRDM i.MX 95 Pro Development Board product page
FRDM i.MX 95 Pro Getting started page
Getting Started with ARA2-M2-16G-GT
Follow the steps below to connect the Ara240 module to the FRDM i.MX 95 Pro development board:
This section will walk you through the Ara240 Runtime software development kit (SDK), a streamlined subset of the Ara240 SDK designed for rapid enablement and execution on NXP platforms. The Runtime SDK simplifies installation and configuration, enabling developers to quickly deploy and run AI/ML workloads on the Ara240 module with minimal effort.
This section provides instructions to verify proper installation of Ara240 module and configuration of the Ara240 Runtime SDK on the FRDM i.MX 95 Pro development board.
Once the board has successfully booted, connect to the serial debug port to monitor system logs. To confirm that the Ara240 module is being detected by the board, run the following command:
$ lspci | grep 1e58
Expected output:
0000:01:00.0 Processing accelerators: Device 1e58:0002 (rev 02)
For quick enablement, the Ara240 Runtime SDK starts at boot time. Refer to the Ara240 Runtime SDK documentation for detailed instructions and environment setup steps.
This section provides an overview of Ara240 runtime software enablement using the FRDM i.MX 95 Pro development board.
Use the following guidance on how to connect required devices. For most of the demos, you would need a camera, keyboard, mouse, internet connection and a HDMI display monitor.
Setup preparation for FRDM i.MX 95 Pro boardSetup preparation for FRDM i.MX 95 Pro board
Runtime SDK delivers a complete runtime environment that enables AI/ML acceleration on the Ara240 module. To run demo applications, ensure that the Ara240 bring-up process has been successfully completed and the system is ready for demo evaluation.
Refer to the Runtime SDK documentation for detailed guidance on:
Following these steps ensures that the module is properly initialized and ready for use. Ara240 supports the execution of CNNs, LLMs, VLMs, and agentic frameworks, enabling advanced AI workloads to run directly on Ara240. For comprehensive examples and end-to-end workflow guidance, please refer to the Ara SDK documentation page.
Henceforth Q2'26 Linux BSP, GoPoint can be launched to explore preselected Ara240 demonstrations included in the NXP provided Linux Board Support Package.
User Guide: GPNTUG: GoPoint for i.MX Applications Processors User Guide