2392000_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2392000_en-US

2392000_en-US

IMXRT 1180 Family

Hello NXP Team,

We are currently evaluating NXP microcontrollers for use in a Space On-Board Computer (OBC) application.

Initially, we were considering the i.MX RT1170 (MIMXRT1170), and during our assessment we noted that NXP documentation specifies that the device is manufactured using 28nm FD-SOI technology. Since semiconductor process technology is a key evaluation criterion for our application, we are now also interested in evaluating the i.MX RT1180 family.

Before proceeding further, we would appreciate clarification regarding the manufacturing process used for the i.MX RT1180:

  • Is the i.MX RT1180 also fabricated using 28nm FD-SOI technology, similar to the i.MX RT1170?
  • If not, could you please provide information on the process technology used for the RT1180?
  • Is there any official documentation or product brief that references the manufacturing node and process technology for this device?

We have reviewed the publicly available documentation but were unable to locate an official statement regarding the RT1180 process technology.

This information is important for our internal technology assessment and qualification activities, and we would greatly appreciate your guidance.

Thank you for your support.

Re: IMXRT 1180 Family

Hi @mayliu1,

Thank you for the quick reply and for confirming that the i.MX RT1180 is manufactured using 28nm FD-SOI technology.

We would appreciate one additional clarification. Could you please confirm whether this applies to the entire i.MX RT1180 family, including the following devices?

  • i.MX RT1186
  • i.MX RT1187
  • i.MX RT1189

If all members of the RT1180 family are fabricated using the same 28nm FD-SOI process, this information will help us proceed with our peripheral and feature analysis to determine the most suitable device for our application.

We would appreciate your confirmation.

Thank you for your support.

Best regards,
Ruthvik R

Re: IMXRT 1180 Family

Hi @ruthvik_1 ,

Thank you so much for your interest in our products and for using our community.

Yes. The i.MX RT1180 uses 28 nm FD-SOI technology .

Sorry, but there is currently no public official documentation or product brief that explicitly references the manufacturing node or process technology for this device.

Wish it helps you

Best Regards,

May

Re: IMXRT 1180 Family

Hi @mayliu1,

Thank you for your prompt response and confirmation. This information is very helpful and greatly appreciated.

Based on your confirmation, we will proceed with our evaluation and consider this as confirmation for the manufacturing technology.

Thank you for your support.

Regards,
Ruthvik R

Re: IMXRT 1180 Family

Hi @ruthvik_1 ,

Thanks for your feedback.

Yes, I checked the information for the i.MX RT1186, i.MX RT1187, and i.MX RT1189. They are all manufactured using the same 28nm FD-SOI process technology.
 
Wish it helps you
Best Regards
May
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-10-2026 03:28 AM
更新者: