Hi,
I am having trouble getting the SD card software going.
All I need to do is get a few items on power-up, no other active management of the SD Card,although I might need logging later on..
I am trying to use data type sd_card_t, and am getting 'unknown type name' error.
I have previously included fsl_sd.h and fsl_sdhc.h. but when I do that I get a multiple definition message for many functions in either. So I assumed that we don't need fsl_sd.h. It isn't even in my SDK, so for the original multiple definiiton error I downloaded both from github. Now I have fsl_sdhc.h from the SDK and am still getting the 'unknown type name' message. Needless to say I am finding the SD card examples very hard to use!
Any help would be very much appreciated!
Hi @ve3id
Thank you for your post,
Please Manage the SDK components in you project and add drivers-> sdhc and middleware->memories->SDMMC Stack->SD
At the sdcard_polling example the following components are included:
carlos_o_0-1783371266922.png
To enter into manage the SDK components you need right click the project and go to SDK Managment -> Manage SDK Components
carlos_o_0-1783371381511.png
Let me know if this solves the issue.
Thank you for the quick reply, Carlos, but I have already done that, so maybe there is something else? Here is my window for the SD management:
ve3id_0-1783426302819.png
Hi @ve3id
Thanks for clarifying,
Could you please share which SDK version you are using?
I tried with 2.11.0 and I'm not able to replicate it at my end.
I am using SDK_2.11.0_FRDM-K64F
I removed it, and built and downloaded a new one of the same version using the "download and install sdks' tab and still have the same problem.
thanks
Nigel