2390237_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2390237_en-US

2390237_en-US

i.MX 943 EVK : Run the ENETC shared use case between Linux and Zephyr

Hello,

I am using the i.MX 943 EVK board and I would like to share the network between the Cortex-A55 SMP on Linux and the Cortex-M33s on Zephyr.

So I got interested in the example :  ENETC shared use case from the i.MX Linux User's Guide (https://www.nxp.com/docs/en/user-guide/UG10163.pdf - Section 11.6.2). This example set an RPMsg connection in order to enable the proxy PF driver on the Linux side. The address of the resource table for the RPMsg connection is 0x208a0000 and the virtqueues are at 0x20800000. These addresses ( [0x20800000 to 0x208A0FFF] ) are located in NETC OCRAM. This region is used as RPMSG shared memory between Cortex-M33 Core1(M33S) and AP(Non Secure Linux).

For this example, I use the mx94evknetc.cfg system manager config file so that the Cortex-M33s have access to the network. Because of this config file, I need to start the A55 and the M33s at boot time, so I use the target imx-mkimage flash_all.


My problem is that when I use a flash_a55 target (with the mx94rte.cfg system manager config file), Linux/U-Boot and Zephyr have access to those addresses but when I switch to flash_all (no matter the system manager config file) neither Linux/U-Boot nor Zephyr have access to those addresses, regardless of the Zephyr program (Zephyr encounters a Bus Fault on these addresses). But if I use any FreeRTOS program such as a simple hello_world instead of Zephyr, the Cortex-M33s and Linux/U-Boot have access to those addresses.

And I can say that if I use a flash_all target with the mx94rte.cfg system manager file,  neither Linux/U-Boot nor Zephyr have access to those addresses but if I stop the Cortex-M33s and load a FreeRTOS hello_world on it and start again, then Linux/U-Boot have access to the NETC OCRAM.

For information, Zephyr doesn't have access with a flash_M33s target.

So I would like to know what FreeRTOS does during its initialization that Zephyr doesn't in order to make the NETC OCRAM accessible between Linux/U-Boot and Zephyr with a flash_all target ?


Zephyr Version : 4.3

Linux Version (Real Time Edge version) : 6.18.2

LinuxRe: i.MX 943 EVK : Run the ENETC shared use case between Linux and Zephyr

Hello @Remantj 

Hope you are doing very well.


Please take a look to the nxp-zephyr Documentation:

https://github.com/nxp-zephyr/nxp-zephyr/blob/main/boards/nxp/imx943_evk/doc/index.rst#programming-a...


Let me know if those changes described in the System-Manager worked in your case.


Best regards,

Salas.

i.MX 943 EVK : Run the ENETC shared use case between Linux and Zephyr

Hello @Manuel_Salas,

Thanks for your answer.

I took a look at the documentation you pointed at, and I tried to patch the System Manager the same way they did in the documentation but nothing has changed.

Which seems kind of expected because the difference in my problem is between a FreeRTOS firmware and a Zephyr firmware. The System Manager config file stays the same between the two cases.

I don't know what FreeRTOS does that Zephyr doesn't regarding the NETC OCRAM but do you have an idea on how to do the same with Zephyr ?

Best regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-10-2026 02:35 AM
更新者: