2390149_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2390149_en-US

2390149_en-US

Could I use any GPIO pin as interrupt input signal which worked at edge detection mode?

Hi,

Because 6 dedicated IRQ(0~5) pins are not enough for me, I need other GPIO pin work as interrupt input signal. So, I have below two questions:

1. Could any GPIO be used as interrupt signal input, which worked at edge detection mode? 

2. If above 1 is yes, what difference between dedicated IRQ and GPIO?  Maybe is response priority?

Thanks in advance!


Best regards!

Jason

Re: Could I use any GPIO pin as interrupt input signal which worked at edge detection mode?

Yes, an LS1021A GPIO can be used as an interrupt input, including edge-detection mode, as long as the pin is actually muxed/available as a GPIO input in your board configuration.

  • GPIO as edge interrupt input
    The GPIO block has interrupt control/status/mask registers: GPIER , GPIMR , and GPICR ; the GPICR configures event detection, including edge-triggered behavior, and the GPIO interrupt logic outputs a consolidated gpio_int request to the system. For each GPIO port line, the EDn bit selects whether the interrupt is generated on any state change or on a high-to-low transition . So GPIO interrupt input is supported, but note that the documented edge choices are not the same as a fully independent rising/falling/both-edge selector: the cited modes are “any change” or “high-to-low.”
  • Dedicated IRQ vs GPIO interrupt
    The main difference is the interrupt path and granularity:
    • Dedicated IRQ0–IRQ5 pins are external I/O signals directly connected to interrupt-controller lines; their interrupt status is available in the corresponding GIC-400 registers, and their polarity is programmable through SCFG_INTPCR .
    • GPIO interrupts are not separate GIC inputs per pin. The GPIO module detects/stores the pin event in GPIER , applies masking/control through GPIO registers, and then drives a consolidated GPIO interrupt request.The reference manual also states that all GPIO interrupts are ORed together for the GPIO interrupt source.

So the practical software difference is that a dedicated IRQ can be handled as its own interrupt source at the GIC level, while a GPIO interrupt normally requires the ISR to enter the GPIO block, read GPIER to determine which pin caused the event, then clear/service it.

Use dedicated IRQ pins for the most latency-sensitive or individually prioritized external interrupts; use GPIO interrupts when you need more inputs and can tolerate shared GPIO interrupt handling.

Re: Could I use any GPIO pin as interrupt input signal which worked at edge detection mode?

Hi,

This question is about LS1021A. Any response is welcome!


Best regards!

Jason

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-08-2026 02:31 AM
更新者: