2390066_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2390066_en-US

2390066_en-US

Regarding the download link for S32K3_RTD_7_0_0

I'm looking to download an RTD executable from the NXP website that meets the following criteria, but I can't find it.
Could you please provide the download link?
I'm in a hurry, so I would appreciate a quick response.

S32K3_RTD_7_0_0_D2510_ASR_REL_4_9_REV_0000_20251031

I found
the following downloadable product, which is similar, but it requires an RTD (Ready-to-Download) that meets the above conditions.

SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP04_HF01_D2510.exe
SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe
SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03_D2512.exe

Re: S32K3_RTD_7_0_0のダウンロードリンクについて

Hi

Do you need to use EBTresos or S32DS?

If you need to use EBTresos, please download and install S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.0 (SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511.exe).

If you need to use S32DS, please download S32K3_S32M27x Real-Time Drivers ASR R23-11 Version 7.0.0 (SW32K3_S32M27x_RTD_R23-11_7.0.0_D2511_DesignStudio_updatesite.zip).

Best Regards,
Robin

Tags (1)
No ratings
Version history
Last update:
‎07-04-2026 02:25 AM
Updated by: