2389831_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389831_en-US

2389831_en-US

Rx sensitivity differs by 10dB between consecutive measurements

I am observing unexpected behavior for one of our products using QN9083 BLE SoC. When I measure the device receiver sensitivity, I am seeing deltas up to 10dB between consecutive measurements. I am using a CMW100 in advertiser mode to perform measurement and the device is placed in a shielded RF box. Performing consecutive RxS measurements, without opening the box and/or changing device location, the device responds with up to 10dB difference (i.e., -91dBm and -81dBm) which is unexpected and never happened before. The behavior is random. I am looking for possible causes both hardware and software.

Re: Rx sensitivity differs by 10dB between consecutive measurements

Hello,


A variation of up to 10 dB between consecutive sensitivity measurements is not something we would normally expect.

Could you share the software/SDK version currently being used?

Also, can you clarify:

Does this occur on a single device or multiple products?

Have you seen the same behavior across different units?

Can the issue be reproduced on an NXP development board using the same measurement setup?

This information will help determine whether the issue is specific to the hardware, software, or test environment.


Best Regards,

Ricardo

Re: Rx sensitivity differs by 10dB between consecutive measurements

Hello thank you for getting back to me. Here are my answers:

Could you share the software/SDK version currently being used?

      5.0 based on 156414 (Controller Subsystem) and 156821 (Host Subsystem)

Does this occur on a single device or multiple products?

      Same product. Never had the issue with different products.

Have you seen the same behavior across different units?

      Yes but not consistently

Can the issue be reproduced on an NXP development board using the same measurement setup?

      I will need a dev board with QN9083 and a FW that will set the chip on advertising

Thank you,


 
 
 
Re: Rx sensitivity differs by 10dB between consecutive measurements

Additional info regarding BLE version:

SDK 2.2.3 BLE 1.5.6 that supports BLE Core 5.0.

Re: Rx sensitivity differs by 10dB between consecutive measurements

@Ricardo_Zamora 

I ran measurements using QN9080-DK. Although I do not see 10dB discrepancy there is still 5dB fluctuation (see data below). What could cause this? 

furbani_0-1784214895282.pngfurbani_0-1784214895282.pngfurbani_0-1784214895282.pngfurbani_0-1784214895282.png


Re: Rx sensitivity differs by 10dB between consecutive measurementsHi @Ricardo_Zamora did you get the chance to look into the data/answers I posted?
Thank you.
Re: Rx sensitivity differs by 10dB between consecutive measurements

I measured the W236 FRDM boards to see how much variation there is in the radiated RSSI. It does vary as much as 4dB.

RomanPBudek_0-1789049903611.pngRomanPBudek_0-1789049903611.pngRomanPBudek_0-1789049903611.pngRomanPBudek_1-1789049923585.pngRomanPBudek_1-1789049923585.pngRomanPBudek_1-1789049923585.png


Re: Rx sensitivity differs by 10dB between consecutive measurements

@RomanPBudek Thank you for the update. What instrument did you use to perform the measurements? I'd like to ship one of our form factor devices if you could measure that one as well.

Thank you

タグ(1)
評価なし
バージョン履歴
最終更新日:
水曜日
更新者: