2389787_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389787_en-US

2389787_en-US

Clarification on sharing Ethernet PHY interrupt pins on i.MX8M Plus

Hi NXP Team,

We are designing an i.MX8M Plus-based SOM with two Ethernet PHYs. Currently, each PHY has a dedicated interrupt GPIO connected to the i.MX8M Plus.

We need clarification on the following:

  1. What are the main software use cases of the Ethernet PHY interrupt pins? Are they mainly used for link up/down, auto-negotiation, speed/duplex change, and Wake-on-LAN events?
  2. Can both Ethernet PHY interrupt outputs be combined and connected to a single i.MX8M Plus GPIO, with software reading both PHY status registers through MDIO to identify the interrupt source?
  3. If direct sharing is not recommended, can one or both Ethernet PHYs be operated using PHY polling without an interrupt pin?
  4. Will using PHY polling affect normal Ethernet data communication, apart from a small delay in detecting link-status changes?

Our intention is to free one GPIO and use it for an ADC data-ready interrupt.

Re: Clarification on sharing Ethernet PHY interrupt pins on i.MX8M Plus

Hello @Sudharsun 

Hope you are doing very well.


What are the main software use cases of the Ethernet PHY interrupt pins? Are they mainly used for link up/down, auto-negotiation, speed/duplex change, and Wake-on-LAN events?

Ethernet PHY interrupt pins are mainly used for PHY event notification such as link up/down, auto-negotiation, speed/duplex changes, and optional Wake-on-LAN events.


Normal Ethernet data traffic does not depend on the interrupt pin. If a PHY interrupt is not provided, Linux PHYLIB can operate the PHY in polling mode.


Can both Ethernet PHY interrupt outputs be combined and connected to a single i.MX8M Plus GPIO, with software reading both PHY status registers through MDIO to identify the interrupt source?

Combining two PHY interrupt outputs into one GPIO may be possible but the safer design is to use polling for one PHY and reserve the GPIO for your ADC DRDY.


Will using PHY polling affect normal Ethernet data communication, apart from a small delay in detecting link-status changes?

Using polling should not affect normal Ethernet communication or throughput.



Best regards,

Salas.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-08-2026 02:30 AM
更新者: